<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Differences between version 6.2 and 6.3 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151511#M3661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys, what are the differences between these two versions ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Nov 2009 23:27:43 GMT</pubDate>
    <dc:creator>Richard777</dc:creator>
    <dc:date>2009-11-04T23:27:43Z</dc:date>
    <item>
      <title>Differences between version 6.2 and 6.3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151511#M3661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys, what are the differences between these two versions ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2009 23:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151511#M3661</guid>
      <dc:creator>Richard777</dc:creator>
      <dc:date>2009-11-04T23:27:43Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between version 6.2 and 6.3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151512#M3662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was going to tell you that such information ought to be present on the CodeWarrior Downloads page, but it is not. I will look into that, but for the sake of getting your question answered, here is what the Welcome_CW_MCUs.txt file has on the subject:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This file contains information about the CodeWarrior Development Studio for Microcontrollers V6.3:&lt;BR /&gt;&lt;BR /&gt;This release provides support for:&lt;BR /&gt;---------------------------------&lt;BR /&gt;&lt;BR /&gt;(1) Newly supported derivatives:&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MC9RS08KB12, MC9RS08KB2, MC9RS08KB4, MC9RS08KB8, MC9RS08LA8, MC9RS08LE4,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MC9S08FL16, MC9S08FL8, SC9S08IA2, SC9S08IA4, SC9S08IB4, SC9S08IB8, SC9S08IC8,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MC9S08JS16, MC9S08JS16L, MC9S08JS8, MC9S08JS8L, MC9S08LG16, MC9S08LG32,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MC9S08LL8, MC9S08LL16, MC9S08LL36, MC9S08LL64, MC9S08MP12, MC9S08MP16,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MC9S08QB4, MC9S08QB8, MC9S08SC4, MC9S08SE4, MC9S08SE8, MC9S08SV16, MC9S08SV8,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF51EM128, MCF51EM256, MCF51JM32, MCF51CN128&lt;BR /&gt;&lt;BR /&gt;(2) Improved version of ColdFire V1 compiler&lt;BR /&gt;&lt;BR /&gt;(3) Evaluation license provided for 30 days evaluation period.&lt;BR /&gt;&lt;BR /&gt;(4) Updated P&amp;amp;E Support.&lt;BR /&gt;&lt;BR /&gt;(5) Support for the new Freescale Open Source BDM connection based on HCS08JM60&lt;BR /&gt;&amp;nbsp; platform. The "HCS08 FSL Open Source BDM" and "CFV1 FSL Open Source BDM" &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; connections can&amp;nbsp;&amp;nbsp; be selected in New Project Wizard for the new derivatives&lt;BR /&gt;&amp;nbsp; listed above.&lt;BR /&gt;&lt;BR /&gt;(6) Debugger support for external memory debugging with MCF51CN128.&lt;BR /&gt;&lt;BR /&gt;(7) Updated Processor Expert 3.07 Release&lt;BR /&gt;&lt;BR /&gt;(8) New CodeWarrior Examples are provided.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;********************************************************&lt;BR /&gt;&lt;BR /&gt;LIMITATIONS:&lt;BR /&gt;-----------&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;WINDOWS VISTA SPECIFIC LIMITATIONS:&lt;BR /&gt;-----------------------------------&lt;BR /&gt;&lt;BR /&gt;The following limitations are applicable only if you are installing the product on Windows Vista:&lt;BR /&gt;&lt;BR /&gt;(1) During installation, security messages may pop up concerning drivers being installed. It is highly&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; recommended to click on the option "continue anyway..", so the drivers can be installed.&lt;BR /&gt;&lt;BR /&gt;(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; with the option to block or unblock the application. It is advisable to click on the unblock option to&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; continue.&lt;BR /&gt;&lt;BR /&gt;(3) For more VISTA specific limitations after the installation, please refer to:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;GENERAL LIMITATIONS:&lt;BR /&gt;--------------------&lt;BR /&gt;&lt;BR /&gt;The following limitations are applicable to Windows Vista, Windows XP:&lt;BR /&gt;&lt;BR /&gt;(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.&lt;BR /&gt;(2) Product supports 32-bit versions of Windows XP, Windows Vista.&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2009 22:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151512#M3662</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-11-06T22:47:53Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between version 6.2 and 6.3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151513#M3663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks very much Jedi Master !!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2009 23:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Differences-between-version-6-2-and-6-3/m-p/151513#M3663</guid>
      <dc:creator>Richard777</dc:creator>
      <dc:date>2009-11-06T23:15:12Z</dc:date>
    </item>
  </channel>
</rss>