<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC9S08QE8 - Sensor Toolbox - AN3922 Code - Hyperterminal in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MC9S08QE8-Sensor-Toolbox-AN3922-Code-Hyperterminal/m-p/145633#M3304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the Sensor Toolbox with MMA8450Q and the USB board. Also I am running the "standard-code" from AN3922 suplied by Freescale. Linking, compiling and flashing is good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is: When I am trying to connect through hyperterminal or similar program (hterm, realterm,...) i can connect, can send a character like "?", but the output from the MCU on the hyperterminal screen is looking like the file enclosed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The register values seems to be correct.&lt;/P&gt;&lt;P&gt;Baudrate is 115200 - - &amp;gt; SCIBD is 0x05 - - &amp;gt; MCU bus freq is 9.216 Mhz - - &amp;gt; 115.2 k,&lt;/P&gt;&lt;P&gt;other registers are standard values.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Settings in hyperterminal are corresponding: Baudrate 115.2 k, Databits 8, Parity None, Stop bits 1, Flow control None, emulationtyp automatic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have an idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Sep 2010 05:26:50 GMT</pubDate>
    <dc:creator>mexxx01</dc:creator>
    <dc:date>2010-09-07T05:26:50Z</dc:date>
    <item>
      <title>MC9S08QE8 - Sensor Toolbox - AN3922 Code - Hyperterminal</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MC9S08QE8-Sensor-Toolbox-AN3922-Code-Hyperterminal/m-p/145633#M3304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the Sensor Toolbox with MMA8450Q and the USB board. Also I am running the "standard-code" from AN3922 suplied by Freescale. Linking, compiling and flashing is good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is: When I am trying to connect through hyperterminal or similar program (hterm, realterm,...) i can connect, can send a character like "?", but the output from the MCU on the hyperterminal screen is looking like the file enclosed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The register values seems to be correct.&lt;/P&gt;&lt;P&gt;Baudrate is 115200 - - &amp;gt; SCIBD is 0x05 - - &amp;gt; MCU bus freq is 9.216 Mhz - - &amp;gt; 115.2 k,&lt;/P&gt;&lt;P&gt;other registers are standard values.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Settings in hyperterminal are corresponding: Baudrate 115.2 k, Databits 8, Parity None, Stop bits 1, Flow control None, emulationtyp automatic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have an idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Sep 2010 05:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MC9S08QE8-Sensor-Toolbox-AN3922-Code-Hyperterminal/m-p/145633#M3304</guid>
      <dc:creator>mexxx01</dc:creator>
      <dc:date>2010-09-07T05:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QE8 - Sensor Toolbox - AN3922 Code - Hyperterminal</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MC9S08QE8-Sensor-Toolbox-AN3922-Code-Hyperterminal/m-p/145634#M3305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to reset a new baud rate based on the MCU frequency of 9.216 Mhz. With the registers I set the baud rate to 9600.&lt;/P&gt;&lt;P&gt;If I try to get a connection with 9600 baud using e.g. hyperterminal the board isn't working, because the working baud rate is 7900.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems, that the MCU frequency is not correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me to check the MCU frequency?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Sep 2010 04:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MC9S08QE8-Sensor-Toolbox-AN3922-Code-Hyperterminal/m-p/145634#M3305</guid>
      <dc:creator>mexxx01</dc:creator>
      <dc:date>2010-09-09T04:16:34Z</dc:date>
    </item>
  </channel>
</rss>