<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I can't set up break points in the source editor(code worrior 5.0) in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143437#M3050</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;anybody can help? please,I can't set up break points in the source editor(code worrior 5.0),I can only do this in the debugger&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;when I click on the left-most column on the line on which I want to break,a red dot indeed appears, but it doesn't stop in the debugger.&lt;/DIV&gt;&lt;DIV&gt;I tried to seek some info in the help menu and found that it say i miss the DAC programm which is said being included in the installation disks under "addons" directory. However, I searched all the disks ,I thaven't found this file,though I indeed found the addons directory.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;please help solve the problem, this feature is very convient and I need this.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks a million.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Harry&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jan 2007 22:21:11 GMT</pubDate>
    <dc:creator>HarrySun</dc:creator>
    <dc:date>2007-01-23T22:21:11Z</dc:date>
    <item>
      <title>I can't set up break points in the source editor(code worrior 5.0)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143437#M3050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;anybody can help? please,I can't set up break points in the source editor(code worrior 5.0),I can only do this in the debugger&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;when I click on the left-most column on the line on which I want to break,a red dot indeed appears, but it doesn't stop in the debugger.&lt;/DIV&gt;&lt;DIV&gt;I tried to seek some info in the help menu and found that it say i miss the DAC programm which is said being included in the installation disks under "addons" directory. However, I searched all the disks ,I thaven't found this file,though I indeed found the addons directory.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;please help solve the problem, this feature is very convient and I need this.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks a million.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Harry&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2007 22:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143437#M3050</guid>
      <dc:creator>HarrySun</dc:creator>
      <dc:date>2007-01-23T22:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: I can't set up break points in the source editor(code worrior 5.0)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143438#M3051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;sorry, I should give more details, I think.&lt;/DIV&gt;&lt;DIV&gt;I am developing a Qg8 based board and use&amp;nbsp;the standard free version of CW.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2007 02:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143438#M3051</guid>
      <dc:creator>HarrySun</dc:creator>
      <dc:date>2007-01-24T02:18:31Z</dc:date>
    </item>
    <item>
      <title>Re: I can't set up break points in the source editor(code worrior 5.0)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143439#M3052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello HarrySun,&lt;BR /&gt;&lt;BR /&gt;It is not possible to get the breakpoint in the source file working in the debugger when working on HC(S)08.&lt;BR /&gt;That is at least what I was told when I had the same issue as you.&lt;BR /&gt;This kind of breakpoint works on some other types of devices though.&lt;BR /&gt;It is not a bug.&lt;BR /&gt;&lt;BR /&gt;A.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2007 16:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143439#M3052</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2007-01-24T16:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: I can't set up break points in the source editor(code worrior 5.0)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143440#M3053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;as Nabla69 says this is simply fact since i use CW for simulating and debugging. If you are debugging this is boring, because you have to set the breakpoints every time when you enter the debugger/simulator. In this case i am writing a command file (*.cmd) with BS commands&lt;BR /&gt;IE BS INI_S (EBS08 entry point) or BS INI_S+1 etc. to clear all breakpoints use BC *.&lt;BR /&gt;&lt;BR /&gt;Saluti Joerg&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I forgot: the command pull down menu is only available if the command window is active!&lt;P&gt;Message Edited by joerg on &lt;SPAN class="date_text"&gt;2007-01-24&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:20 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2007 18:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/I-can-t-set-up-break-points-in-the-source-editor-code-worrior-5/m-p/143440#M3053</guid>
      <dc:creator>joerg</dc:creator>
      <dc:date>2007-01-24T18:18:22Z</dc:date>
    </item>
  </channel>
</rss>