<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PK-HCS12E128 + VMWARE in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/PK-HCS12E128-VMWARE/m-p/143407#M3042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I was hoping to use VMware also as I have a MAC. Using the P&amp;amp;E usb pod I was able to burn but it died right after that. I since got the AW60 demo board and the usb interface is detected but the script errors with code 45. I think during the loading of the scripts the usb disconnects then reconnects and that causes a problem.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Nov 2007 08:27:45 GMT</pubDate>
    <dc:creator>jamesarm97</dc:creator>
    <dc:date>2007-11-17T08:27:45Z</dc:date>
    <item>
      <title>PK-HCS12E128 + VMWARE</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/PK-HCS12E128-VMWARE/m-p/143406#M3041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Has anyone got CW / Datablaze etc. working with a usb link when Windows is hosted by VMWare under Linux?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My setup uses&amp;nbsp;VMWare Server and it&amp;nbsp;seems like it's going to&amp;nbsp;work (ie: the controller halts when CW tries to communicate with it) but nothing else happens and CW / Datablaze&amp;nbsp;just hang until the usb lead is disconnected.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I&amp;nbsp;suspect it's not an easy problem to fix!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2007 22:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/PK-HCS12E128-VMWARE/m-p/143406#M3041</guid>
      <dc:creator>onamatic</dc:creator>
      <dc:date>2007-08-20T22:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: PK-HCS12E128 + VMWARE</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/PK-HCS12E128-VMWARE/m-p/143407#M3042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I was hoping to use VMware also as I have a MAC. Using the P&amp;amp;E usb pod I was able to burn but it died right after that. I since got the AW60 demo board and the usb interface is detected but the script errors with code 45. I think during the loading of the scripts the usb disconnects then reconnects and that causes a problem.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Nov 2007 08:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/PK-HCS12E128-VMWARE/m-p/143407#M3042</guid>
      <dc:creator>jamesarm97</dc:creator>
      <dc:date>2007-11-17T08:27:45Z</dc:date>
    </item>
  </channel>
</rss>