<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Project settings wrong for debug mode in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142544#M2891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;from what I can see both project were loaded correctly. But I assume that your second project code has something in it which let the application crash or run away?&lt;BR /&gt;I believe you would have to provide some more details on this one about what is happening?&lt;BR /&gt;&lt;BR /&gt;Erich&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Aug 2007 20:32:12 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2007-08-09T20:32:12Z</dc:date>
    <item>
      <title>Project settings wrong for debug mode</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142543#M2890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am brand new to codewarrior.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have several assembly code projects that need to be tweeked.&amp;nbsp; I've was given one project as a guideline, the rest I was just given the asm files.&amp;nbsp;&amp;nbsp; I can't seem to find the settings that let the origninal project load into the BDM for the debug.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;The project that works list this in the cmd box&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.55&lt;BR /&gt;Frequency change to ~8050304hz.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.55&lt;BR /&gt;Device is 9S08RG60.&lt;BR /&gt;Mode is In-Circuit Debug.&lt;/P&gt;&lt;P&gt;IO registers loaded for MC9S08RG60 from C:\Program Files\Freescale\CodeWarrior for HC08 V5.1\prog\REG\MCU1014.REG&lt;BR /&gt;Startup command file does not exist.&lt;BR /&gt;Preload command file does not exist.&lt;/P&gt;&lt;P&gt;Loading 59900 bytes.&lt;BR /&gt;Postload command file does not exist.&lt;BR /&gt;STARTED&lt;BR /&gt;RUNNING&lt;/P&gt;&lt;P&gt;in&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is what comes up in the cmd box for the file that doesn't load&lt;/STRONG&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;executing ASM_layout.hwl&lt;/P&gt;&lt;P&gt;!OPEN source 0 0 60 42&lt;BR /&gt;NO CONNECTION&lt;BR /&gt;!Source &amp;lt; attributes MARKS off&lt;BR /&gt;!OPEN assembly 60 0 40 30&lt;BR /&gt;!Assembly &amp;lt; attributes ADR on,CODE off,ABSADR on,SYMB off,TOPPC 0xF800&lt;BR /&gt;!OPEN procedure 60 60 40 17&lt;BR /&gt;!Procedure &amp;lt; attributes VALUES on,TYPES off&lt;BR /&gt;!OPEN register 60 30 40 30&lt;BR /&gt;!Register &amp;lt; attributes FORMAT AUTO,COMPLEMENT None&lt;BR /&gt;!OPEN memory 60 77 40 23&lt;BR /&gt;!Memory &amp;lt; attributes FORMAT hex,COMPLEMENT None,WORD 1,ASC on,ADR on,ADDRESS 0x80&lt;BR /&gt;!OPEN data 0 42 60 28&lt;BR /&gt;!Data &amp;lt; attributes SCOPE global,COMPLEMENT None,FORMAT Symb,MODE automatic,UPDATERATE 10,NAMEWIDTH 16&lt;BR /&gt;!OPEN command 0 70 60 30&lt;BR /&gt;!Command &amp;lt; attributes CACHESIZE 1000&lt;BR /&gt;!bckcolor 50331647&lt;BR /&gt;!font 'Courier New' 9 BLACK&lt;BR /&gt;!AUTOSIZE on&lt;BR /&gt;!ACTIVATE Assembly Memory Register Command Data Source Procedure&amp;nbsp;&lt;BR /&gt;done ASM_layout.hwl&lt;/P&gt;&lt;P&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.55&lt;BR /&gt;Frequency change to ~8050304hz.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.55&lt;BR /&gt;WARNING - Device is secure. Flash is not accessible.&lt;BR /&gt;Device is 9S08RG60.&lt;BR /&gt;Mode is In-Circuit Debug.&lt;/P&gt;&lt;P&gt;IO registers loaded for MC9S08RG60 from C:\Program Files\Freescale\CodeWarrior for HC08 V5.1\prog\REG\MCU1014.REG&lt;BR /&gt;executing .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_startup.cmd&lt;/P&gt;&lt;P&gt;!// At startup the commands written below will be executed&lt;BR /&gt;Target Ready&lt;BR /&gt;done .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_startup.cmd&lt;/P&gt;&lt;P&gt;Startup command file correctly executed.&lt;BR /&gt;executing .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_preload.cmd&lt;/P&gt;&lt;P&gt;!// Before load the commands written below will be executed&lt;BR /&gt;done .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_preload.cmd&lt;/P&gt;&lt;P&gt;Preload command file correctly executed.&lt;/P&gt;&lt;P&gt;Loading 47777 bytes.&lt;BR /&gt;executing .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_postload.cmd&lt;/P&gt;&lt;P&gt;!// After load the commands written below will be executed&lt;BR /&gt;MCU Device Selection has been changed.&lt;BR /&gt;done .\cmd\BDM_P&amp;amp;E_Multilink_CyclonePro_postload.cmd&lt;/P&gt;&lt;P&gt;Postload command file correctly executed.&lt;BR /&gt;STARTED&lt;BR /&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I've tried copying the project to another folder and then replacing the ASM files.&amp;nbsp; This gave me lots of errors, so then I tried creating a new project and removing the main.asm and putting in my asm files and this doesn't give me errors, it just doesn't load the object code into the BDM.&lt;/P&gt;&lt;P&gt;Can anyone shed any light?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2007 20:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142543#M2890</guid>
      <dc:creator>Vickyg</dc:creator>
      <dc:date>2007-08-09T20:09:31Z</dc:date>
    </item>
    <item>
      <title>Re: Project settings wrong for debug mode</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142544#M2891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;from what I can see both project were loaded correctly. But I assume that your second project code has something in it which let the application crash or run away?&lt;BR /&gt;I believe you would have to provide some more details on this one about what is happening?&lt;BR /&gt;&lt;BR /&gt;Erich&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2007 20:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142544#M2891</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2007-08-09T20:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: Project settings wrong for debug mode</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142545#M2892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;The second project doesn't show me what's in memory, or if it does, memory is all 0's.&amp;nbsp; The assembly code shown in the debug assembly&amp;nbsp;window, doesn't have anything to do with the source code shown in the source window.&amp;nbsp;&amp;nbsp; It appears to be trying to execute 00 00 00.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So I have some sort of setting wrong to allow&amp;nbsp;me to load flash and enter debug correctly, or I have some protection on in the assembly listing.&amp;nbsp; I'm think the cmd listings are giving me a clue, I just don't have enough experience with codewarrior to figure it out.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2007 21:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142545#M2892</guid>
      <dc:creator>Vickyg</dc:creator>
      <dc:date>2007-08-09T21:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: Project settings wrong for debug mode</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142546#M2893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Never mind.&amp;nbsp; I was confused about the security bit vs enable background settings.&amp;nbsp; Found the security bit and now I can see to debug.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2007 07:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Project-settings-wrong-for-debug-mode/m-p/142546#M2893</guid>
      <dc:creator>Vickyg</dc:creator>
      <dc:date>2007-08-10T07:23:52Z</dc:date>
    </item>
  </channel>
</rss>