<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: QT1A Full Chip Simulation in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141139#M2634</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thankyou for the information.&lt;BR /&gt;&lt;BR /&gt;I've also tierd with CW5.1 and the QY4A update with the same result.&lt;BR /&gt;&lt;BR /&gt;I'll be waiting for news from P&amp;amp;E.&lt;BR /&gt;&lt;BR /&gt;Bye.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Jun 2006 20:12:11 GMT</pubDate>
    <dc:creator>StefanoQ</dc:creator>
    <dc:date>2006-06-27T20:12:11Z</dc:date>
    <item>
      <title>QT1A Full Chip Simulation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141137#M2632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm developing an application for the QT1A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to simulate the application with the CodeWarrior debugger.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My application uses the KBI interrupt and the possibility to select its polarity using the KBIPR register.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The debugger shows me the register in the data window but it stops when the program tries to write a value into the register with the message 'Error: At location 001C - &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error: Attempt to use unimplemented (--) memory.'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've already installed the update for CW3.1 related to QY4A but with no effect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I thinkis a problem in the memory definition for the CPU. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do anyone know how to overcome the problem or if there's a new update for the CW3.1?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Stefano Quadri&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 17:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141137#M2632</guid>
      <dc:creator>StefanoQ</dc:creator>
      <dc:date>2006-06-27T17:53:53Z</dc:date>
    </item>
    <item>
      <title>Re: QT1A Full Chip Simulation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141138#M2633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp; I assume you are using full chip simulation. Am I right?&lt;/P&gt;&lt;P&gt;Full chip simulation for diverse HC08 MCU are missing simulation of KBIPR register.I have already reported that to P&amp;amp;E asking them for a fix.&lt;/P&gt;&lt;P&gt;In the mean time I can only advise you to use the real hardware for debugging.&lt;/P&gt;&lt;P&gt;Also note that the HC908QT4A is only supported with CodeWarrior for HC(S)08 V5.1 after you install the appropriate service pack.&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 19:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141138#M2633</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-06-27T19:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: QT1A Full Chip Simulation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141139#M2634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thankyou for the information.&lt;BR /&gt;&lt;BR /&gt;I've also tierd with CW5.1 and the QY4A update with the same result.&lt;BR /&gt;&lt;BR /&gt;I'll be waiting for news from P&amp;amp;E.&lt;BR /&gt;&lt;BR /&gt;Bye.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 20:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141139#M2634</guid>
      <dc:creator>StefanoQ</dc:creator>
      <dc:date>2006-06-27T20:12:11Z</dc:date>
    </item>
    <item>
      <title>Re: QT1A Full Chip Simulation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141140#M2635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;The simulation issue is not fixed in V5.1 with service pack. But at least with V5.1 and service pack installed you should be able to debug on real hardware.&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 20:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/QT1A-Full-Chip-Simulation/m-p/141140#M2635</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-06-27T20:52:40Z</dc:date>
    </item>
  </channel>
</rss>