<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where is the ROM_LIB keyword generated .S19 file? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Where-is-the-ROM-LIB-keyword-generated-S19-file/m-p/141134#M2631</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi bennyxu,&lt;BR /&gt;&lt;BR /&gt;AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.&lt;BR /&gt;Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.&lt;BR /&gt;If you are building with a makefile, use the burner.exe to create an SRecord.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Dec 2006 21:20:59 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2006-12-27T21:20:59Z</dc:date>
    <item>
      <title>Where is the ROM_LIB keyword generated .S19 file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Where-is-the-ROM-LIB-keyword-generated-S19-file/m-p/141133#M2630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;LINK ROMLIB.lib AS ROM_LIB&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;generated .s19 file very small.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;HOW to used to "ROM_LIB"&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Dec 2006 15:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Where-is-the-ROM-LIB-keyword-generated-S19-file/m-p/141133#M2630</guid>
      <dc:creator>bennyxu</dc:creator>
      <dc:date>2006-12-26T15:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the ROM_LIB keyword generated .S19 file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Where-is-the-ROM-LIB-keyword-generated-S19-file/m-p/141134#M2631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi bennyxu,&lt;BR /&gt;&lt;BR /&gt;AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.&lt;BR /&gt;Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.&lt;BR /&gt;If you are building with a makefile, use the burner.exe to create an SRecord.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Dec 2006 21:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Where-is-the-ROM-LIB-keyword-generated-S19-file/m-p/141134#M2631</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-12-27T21:20:59Z</dc:date>
    </item>
  </channel>
</rss>