<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: plz help using interrupt</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/plz-help-using-interrupt/m-p/140954#M2595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;Just giving some documentation hints:&lt;BR /&gt;I suggest that you first have a look into the compiler manual (in the Help\pdf subfolder). There is information about how to tell the compiler to generate code for interrupt service routines. You can search for #pragma TRAP_PROC or how to use the 'interrupt' keyword.&lt;BR /&gt;&lt;BR /&gt;If you are using the TRAP_PROC way or interrupt without a vector number, you need to tell the linker where to allocate the vectors. See the linker manual and and see the things about 'VECTOR'.&lt;BR /&gt;&lt;BR /&gt;Erich&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Jun 2006 16:58:25 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2006-06-27T16:58:25Z</dc:date>
    <item>
      <title>plz help using interrupt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/plz-help-using-interrupt/m-p/140953#M2594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;hi,&lt;/DIV&gt;&lt;DIV&gt;i want to use interrupt on Serial recieive(ESCI) i am using QB8 4.9152Mhz crystal&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;plz guide where and how to write the interrupt routine and what r thr various setting or any line i have to write to enable and use interrupt&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;in interupt(RX of ESCI) i want to say tx some byte.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;#include &amp;lt;hidef.h&amp;gt; /* for EnableInterrupts macro */&lt;BR /&gt;#include &amp;lt;MC68HC908QB4.h&amp;gt; /* include peripheral declarations */&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;//macro defination for PORTB out&lt;BR /&gt;#define setbit(A,B) A|=(1&amp;lt;&amp;lt;B)&lt;BR /&gt;#define clrbit(A,B) A&amp;amp;=~(1&amp;lt;&amp;lt;B)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;void uart_init(void)&lt;BR /&gt;{&lt;/DIV&gt;&lt;DIV&gt;setbit(DDRB,5);&amp;nbsp; //TX as output&lt;BR /&gt;clrbit(DDRB,4);&amp;nbsp; //RX as input&lt;/DIV&gt;&lt;DIV&gt;SCC1=0x40;&lt;BR /&gt;SCC2=0x0c;&lt;BR /&gt;SCC3=0x00;&lt;BR /&gt;SCBR=0x00;&lt;BR /&gt;SCPSC=0xE0;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;void uart_sendbyte(unsigned char byte)&lt;BR /&gt;{&lt;BR /&gt;while(!SCS1_SCTE);&lt;BR /&gt;while(!SCS1_TC);&lt;BR /&gt;SCDR=byte;&lt;BR /&gt;while(!SCS1_TC);&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;unsigned char uart_rxbyte(void)&lt;BR /&gt;{&lt;BR /&gt;unsigned char byte;&lt;BR /&gt;while(!SCS1_SCRF);&lt;BR /&gt;byte=SCDR;&lt;BR /&gt;return byte;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void delay(unsigned int cycles)&lt;BR /&gt;{&lt;BR /&gt;while(cycles) cycles--;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;void adc_init()&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp; ADCLK = 0x24;&lt;BR /&gt;&amp;nbsp; ADSCR = 0x1F;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;unsigned int&amp;nbsp; adc(unsigned char channel)&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; unsigned int adc_value;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; ADSCR |= channel;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; delay(100);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while(!ADSCR_COCO);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; adc_value=(ADRH&amp;lt;&amp;lt;8);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; adc_value=adc_value+ADRL;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; return adc_value;&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;void main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; CONFIG1=0x01;//disable COP&lt;BR /&gt;&amp;nbsp; delay(1000);&lt;BR /&gt;&amp;nbsp; OSCSC=0xC4;&lt;BR /&gt;&amp;nbsp; delay(100);&lt;BR /&gt;&amp;nbsp; OSCSC |=0x02;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; //PTB0=analog input&lt;BR /&gt;&amp;nbsp; //PTB1=Fault digittal input&lt;BR /&gt;&amp;nbsp; //PTB4=RX RS232 INPUT&lt;BR /&gt;&amp;nbsp; //PTB5=TX RS232 OUTPUT&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; DDRB = 0x00;//All INPUT INITIALLY&lt;BR /&gt;&amp;nbsp; uart_init();&lt;BR /&gt;&amp;nbsp;adc_init();&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; while(1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uart_sendbyte(0xAA);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; delay(500);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;please guide me with some example code&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks and regards&lt;/DIV&gt;&lt;DIV&gt;Pallav Aggarwal&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2006 14:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/plz-help-using-interrupt/m-p/140953#M2594</guid>
      <dc:creator>pallav</dc:creator>
      <dc:date>2006-06-26T14:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: plz help using interrupt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/plz-help-using-interrupt/m-p/140954#M2595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;Just giving some documentation hints:&lt;BR /&gt;I suggest that you first have a look into the compiler manual (in the Help\pdf subfolder). There is information about how to tell the compiler to generate code for interrupt service routines. You can search for #pragma TRAP_PROC or how to use the 'interrupt' keyword.&lt;BR /&gt;&lt;BR /&gt;If you are using the TRAP_PROC way or interrupt without a vector number, you need to tell the linker where to allocate the vectors. See the linker manual and and see the things about 'VECTOR'.&lt;BR /&gt;&lt;BR /&gt;Erich&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 16:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/plz-help-using-interrupt/m-p/140954#M2595</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2006-06-27T16:58:25Z</dc:date>
    </item>
  </channel>
</rss>