<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Timers...</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140796#M2534</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using CW v5, HC08GZ&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if a delay is used as shown below, how long is the delay in real time ? Say if the clock is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;8 Mhz, is it as simple as dividing the counter by 8e6 to get real time delay ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;for(cnt2 = 35535; cnt2 != 0; cnt2--);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or could the following CPU delay function generated by CPU bean could be used ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void Cpu_Delay100US(word us100)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;for example, if a 1 ms delay is needed, 10 would be use as an argument ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;appreciate any help i can get.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Dec 2006 01:43:30 GMT</pubDate>
    <dc:creator>tmyint</dc:creator>
    <dc:date>2006-12-21T01:43:30Z</dc:date>
    <item>
      <title>Timers...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140796#M2534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using CW v5, HC08GZ&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if a delay is used as shown below, how long is the delay in real time ? Say if the clock is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;8 Mhz, is it as simple as dividing the counter by 8e6 to get real time delay ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;for(cnt2 = 35535; cnt2 != 0; cnt2--);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or could the following CPU delay function generated by CPU bean could be used ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void Cpu_Delay100US(word us100)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;for example, if a 1 ms delay is needed, 10 would be use as an argument ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;appreciate any help i can get.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2006 01:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140796#M2534</guid>
      <dc:creator>tmyint</dc:creator>
      <dc:date>2006-12-21T01:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: Timers...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140797#M2535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For a simple timing loop delay there will be many cycles per loop, depending on the code that the compiler generates.&amp;nbsp; The easiest way to "calibrate" the loop is to simulate operation using the debugger.&amp;nbsp; Simply note the CPU cycles just prior to entering the loop, and immediately after leaving the loop, and subtract the two values.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;To test your code, I needed to use the following to prevent timeout of the COP timer -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;word cnt2;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;for (cnt2 = 35535; cnt2 != 0; cnt2--)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;__RESET_WATCHDOG();&lt;BR /&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;To execute the loop with HC08 device required a total of 782193 bus cycles, or about 22 cycles per loop.&amp;nbsp;The total delay will increase should any interrupts occur.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Incidently, using an incrementing loop (rather than decrementing) actually required about 28 cycles per loop.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2006 09:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140797#M2535</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-12-21T09:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: Timers...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140798#M2536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;hey bigmac,&lt;BR /&gt;&lt;BR /&gt;i had the same code to prevent the timeout, sorry I didnt care to put it in, but thanks for your help. so i guess my final question is, wat is the difference between using the loop cycle delay and CPU delay that generated by the CPU bean ?&lt;BR /&gt;&lt;BR /&gt;Thet&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2006 00:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timers/m-p/140798#M2536</guid>
      <dc:creator>tmyint</dc:creator>
      <dc:date>2006-12-22T00:42:03Z</dc:date>
    </item>
  </channel>
</rss>