<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Code Warrior True-Time Simulator &amp; Debugger</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-True-Time-Simulator-Debugger/m-p/140647#M2513</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using Code Warrior which came with the DEMO9S08AW60E Evaluation Board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I load an S19 file into the debugger, a dialog appears which says:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Load Image contains flash memory data", "Erase and program flash?"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I&amp;nbsp; click "YES" and&amp;nbsp; the&amp;nbsp; CPROGHCS08 Programmer window appears.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The program automatically executes;&amp;nbsp; CM, EM, and PM, however, when the PM (Program Module) is executed,&amp;nbsp; I get the following error message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Programming and verifying address&amp;nbsp; $01860 Error during programming."&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Error 18 during script"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In other posts I have read a suggestion to use the "Expert Mode Programmer"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I use the Expert Mode Programmer, and perform Erase Module, and Program Module, I get no error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Question:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why at this level of maturity for this product does the Erase and Program function&amp;nbsp; within the True-Time Simulator and Debugger not work?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jul 2007 03:47:13 GMT</pubDate>
    <dc:creator>CaptMike2452</dc:creator>
    <dc:date>2007-07-20T03:47:13Z</dc:date>
    <item>
      <title>Code Warrior True-Time Simulator &amp; Debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-True-Time-Simulator-Debugger/m-p/140647#M2513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using Code Warrior which came with the DEMO9S08AW60E Evaluation Board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I load an S19 file into the debugger, a dialog appears which says:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Load Image contains flash memory data", "Erase and program flash?"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I&amp;nbsp; click "YES" and&amp;nbsp; the&amp;nbsp; CPROGHCS08 Programmer window appears.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The program automatically executes;&amp;nbsp; CM, EM, and PM, however, when the PM (Program Module) is executed,&amp;nbsp; I get the following error message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Programming and verifying address&amp;nbsp; $01860 Error during programming."&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Error 18 during script"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In other posts I have read a suggestion to use the "Expert Mode Programmer"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I use the Expert Mode Programmer, and perform Erase Module, and Program Module, I get no error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Question:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why at this level of maturity for this product does the Erase and Program function&amp;nbsp; within the True-Time Simulator and Debugger not work?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2007 03:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-True-Time-Simulator-Debugger/m-p/140647#M2513</guid>
      <dc:creator>CaptMike2452</dc:creator>
      <dc:date>2007-07-20T03:47:13Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior True-Time Simulator &amp; Debugger</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-True-Time-Simulator-Debugger/m-p/140648#M2514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Mike,&lt;BR /&gt;&lt;BR /&gt;Unfortunately you forgot to read the &lt;B&gt;&amp;nbsp; &lt;A class="subj_read" href="http://forums.freescale.com/message?board.id=CWCOMM&amp;amp;message.id=3819" rel="nofollow" target="_blank"&gt;[IMPORTANT] When Asking about CODEWARRIOR !!!&lt;/A&gt;&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;There is a crucial point missing: the version you are using + which cable ?!&lt;BR /&gt;Please come back with it.&lt;BR /&gt;&lt;BR /&gt;The product you use has been tested and is supposed to work.&lt;BR /&gt;I don't see any product that is recognizing the S08AW60 and would not program it, that is a basic S08 product in term of programming and is supported.&lt;BR /&gt;&lt;BR /&gt;The language you use let me thinh you are using the USB Multilink from P&amp;amp;E Microcomputers + their associated "third party" software add-on to CodeWarrior. But the rest is doesn't come to my crystal ball &lt;SPAN&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2007 17:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Code-Warrior-True-Time-Simulator-Debugger/m-p/140648#M2514</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-07-23T17:45:04Z</dc:date>
    </item>
  </channel>
</rss>