<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: i have a problem with the debug</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140211#M2438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi effrit,&lt;BR /&gt;&lt;BR /&gt;on the link you copied the firmware is defininig the reset vector:&lt;BR /&gt;out of VECJB8.C:&lt;BR /&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;extern void isrDummy(void);extern void isrUSB(void);extern void isrKey(void);extern void _Startup(void);//-- Interrupt Vector Table --------------------------------------------------void (* const _vectab[])(void) @0xFFF0 = {    isrKey,                    /* Keypad             */    isrDummy,                /* TIMER overflow    */    isrDummy,                /* TIMER channel 1    */    isrDummy,                /* TIMER channel 0    */    isrDummy,                /* IRQ1              */    isrUSB,                    /* USB                */    isrDummy,                /* SWI                 */    _Startup            /* RESET            */    };&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;So that should do it. Which version of the code did you start with? A zip supporting CW?&lt;BR /&gt;&lt;BR /&gt;Well, anyway, in the end I know the tools but I did never use (or even try to use) this USB chip, so I cannot really help for specific questions.&lt;BR /&gt;I wonder also what is the problem you try to solve?&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;/DIV&gt;&lt;A href="http://forums.freescale.com/../view_profile?user.id=8024" rel="nofollow noopener noreferrer noopener noreferrer" target="top"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 08:40:23 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2020-10-29T08:40:23Z</dc:date>
    <item>
      <title>CW6.0 HC908JB8 - i have a problem with the debug</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140208#M2435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;hi, i try to debug an example code but when i push start the command window said me :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Windows NT detected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Simulated device is HC908JB8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Warning - Reset Vector not initialized.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Device is HC908JB8.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mode is Full Chip Simulation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;IO registers loaded for MC68HC908JB8 from C:\Archivos de programa\Freescale\CodeWarrior for Microcontrollers V6.0\prog\REG\HC908JB8.REG&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Startup command file does not exist.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Preload command file does not exist.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Postload command file does not exist.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Target Ready&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RESET&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A power-on Reset has occured.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;STARTED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RUNNING&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I do not understand the failure because all the files are loaded correctly and none is absent.what can i do??? thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;BR /&gt;Alban Edit: FSL Part Number + CW version must figure in Message Subject line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by Alban on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-07-23&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:46 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2007 21:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140208#M2435</guid>
      <dc:creator>effrit</dc:creator>
      <dc:date>2007-07-16T21:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: i have a problem with the debug</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140209#M2436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I would fix the&lt;BR /&gt;&amp;gt;Warning - Reset Vector not initialized.&lt;BR /&gt;warning, basically the reset vector is how the application will start if there is no debugger, so that's important :smileyhappy:&lt;BR /&gt;&lt;BR /&gt;About the reset of the messages, well looks like the debugger is a bit noisy. But those messages do not mean anything in particular is wrong.&lt;BR /&gt;That you do not have those command files is not a problem, I would say it's more the normal setup these days than to actually have those command files.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2007 22:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140209#M2436</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-07-16T22:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: i have a problem with the debug</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140210#M2437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thanks daniel for reply me,i sorry because my english is not very good,i´m from spain.&lt;BR /&gt;i can make another question.how i can initialezed the vectors? i try to explain i am compile a code for usb hc08 and all code are make but i have to debug for simulate the board,the code i download to &lt;A href="http://elmicro.com/hc08web/usb08/index.html.i" target="test_blank"&gt;http://elmicro.com/hc08web/usb08/index.html.i&lt;/A&gt; will been very grateful with that someone was helping. THANKS&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2007 22:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140210#M2437</guid>
      <dc:creator>effrit</dc:creator>
      <dc:date>2007-07-16T22:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: i have a problem with the debug</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140211#M2438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi effrit,&lt;BR /&gt;&lt;BR /&gt;on the link you copied the firmware is defininig the reset vector:&lt;BR /&gt;out of VECJB8.C:&lt;BR /&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;extern void isrDummy(void);extern void isrUSB(void);extern void isrKey(void);extern void _Startup(void);//-- Interrupt Vector Table --------------------------------------------------void (* const _vectab[])(void) @0xFFF0 = {    isrKey,                    /* Keypad             */    isrDummy,                /* TIMER overflow    */    isrDummy,                /* TIMER channel 1    */    isrDummy,                /* TIMER channel 0    */    isrDummy,                /* IRQ1              */    isrUSB,                    /* USB                */    isrDummy,                /* SWI                 */    _Startup            /* RESET            */    };&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;So that should do it. Which version of the code did you start with? A zip supporting CW?&lt;BR /&gt;&lt;BR /&gt;Well, anyway, in the end I know the tools but I did never use (or even try to use) this USB chip, so I cannot really help for specific questions.&lt;BR /&gt;I wonder also what is the problem you try to solve?&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;/DIV&gt;&lt;A href="http://forums.freescale.com/../view_profile?user.id=8024" rel="nofollow noopener noreferrer noopener noreferrer" target="top"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140211#M2438</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2020-10-29T08:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: i have a problem with the debug</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140212#M2439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;hi daniel,thanks for help me.i try to run the version &lt;A href="http://elmicro.com/hc08web/usb08/files/usb08_fwv101_metrowerks.zip" rel="nofollow" target="_blank"&gt;USB08 Firmware V1.01 for Metrowerks Codewarrior&lt;/A&gt; i have to run this project only but the project failed and i don´t know when he failed.if you can try to run the project and see if he run good or he failed.1º i unzip the files and after i open the file HC08 USB.mcp and CW start,after i click debug and i choice hc08 full simulation and the chip is hc908jb8.and when i click start in the command windows i can see failed.Daniel and the other version of fireware failed to.&lt;BR /&gt;Thanks very much Daniel because the fireware it´s turning me crazy&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2007 21:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW6-0-HC908JB8-i-have-a-problem-with-the-debug/m-p/140212#M2439</guid>
      <dc:creator>effrit</dc:creator>
      <dc:date>2007-07-19T21:38:03Z</dc:date>
    </item>
  </channel>
</rss>