<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 CW HC(S)08 5.1 - New Project wizard</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-HC-S-08-5-1-New-Project-wizard/m-p/125686#M234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Some feedback on the new project wizard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I really hate not being able to add multiple files with the otion "add existing files to the project". That is, you need to select them individually.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I'm used to, is being able to do multiple file selection. Perhaps a button for "add existing files", which would use a standard Windows dialog for open/save files. Usign the standard dialog gives you access to the date/time as well as file type.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The current embedded explorer view is quite lacking. You can see what file types they are (.c or .h), you can't see what the date/time is, as well as not being able to select multiple files. Typicaly, I'd like to be able to select all files in a folder, but you can't do that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The CW IDE is quite nice. Vastly superior to what I'm trying to migrate away from. But there are quite a few things I think it's lacking. Most of them are basic features, and really not difficult to include.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Aug 2006 20:50:33 GMT</pubDate>
    <dc:creator>Bruce_andrew</dc:creator>
    <dc:date>2006-08-03T20:50:33Z</dc:date>
    <item>
      <title>CW HC(S)08 5.1 - New Project wizard</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-HC-S-08-5-1-New-Project-wizard/m-p/125686#M234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Some feedback on the new project wizard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I really hate not being able to add multiple files with the otion "add existing files to the project". That is, you need to select them individually.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I'm used to, is being able to do multiple file selection. Perhaps a button for "add existing files", which would use a standard Windows dialog for open/save files. Usign the standard dialog gives you access to the date/time as well as file type.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The current embedded explorer view is quite lacking. You can see what file types they are (.c or .h), you can't see what the date/time is, as well as not being able to select multiple files. Typicaly, I'd like to be able to select all files in a folder, but you can't do that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The CW IDE is quite nice. Vastly superior to what I'm trying to migrate away from. But there are quite a few things I think it's lacking. Most of them are basic features, and really not difficult to include.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2006 20:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-HC-S-08-5-1-New-Project-wizard/m-p/125686#M234</guid>
      <dc:creator>Bruce_andrew</dc:creator>
      <dc:date>2006-08-03T20:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: CW HC(S)08 5.1 - New Project wizard</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-HC-S-08-5-1-New-Project-wizard/m-p/125687#M235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank you for the valuable feedback.&lt;/DIV&gt;&lt;DIV&gt;I have internally forwarded your suggestions for improvement to the product manager.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2006 15:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-HC-S-08-5-1-New-Project-wizard/m-p/125687#M235</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-08-15T15:11:54Z</dc:date>
    </item>
  </channel>
</rss>