<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: L1100 linker errors with CodeWarrior HC12 toolchain</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/L1100-linker-errors-with-CodeWarrior-HC12-toolchain/m-p/137405#M1996</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've seen this slew of errors when I use the CodeWarrior project wizard to build the HC12 version of OSEK. OSEK provides its own HC12 header information. Those files, along with the standard boiler-plate headers the CodeWarrior project provides, create redundant definitions. What you are seeing is the linker complaining of these redundant definitions.&lt;BR /&gt;&lt;BR /&gt;You're either going to have to live with the other software's header files, or carefully edit the CodeWarrior header file to include only the information that the other header files lack.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 May 2006 20:52:59 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2006-05-30T20:52:59Z</dc:date>
    <item>
      <title>L1100 linker errors with CodeWarrior HC12 toolchain</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/L1100-linker-errors-with-CodeWarrior-HC12-toolchain/m-p/137404#M1995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the CodeWarrior HC12 toolchain V5.0.28 Build 5073. My project is based on standard software modules from different companies, so I can't change the source code. One software module is using a microcontroller register definition file for the MC9S12XDP512 (called Reg_xdp512.h). This file doesn't suit my needs (too few or missing bit and mask definitions etc.) and I want to use "mc9s12xdp512.h" from _CODEWARRIOR_DIR_\lib\hc12c\include.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As soon, as I include this file in my sources, I get the following warnings:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg0 (0x0) and .absSeg652 (0x0) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg652 (0x0) and .absSeg1168 (0x0) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1168 (0x0) and .absSeg1820 (0x0) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1820 (0x0) and .absSeg653 (0x1) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1 (0x2) and .absSeg654 (0x2) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg654 (0x2) and .absSeg1169 (0x2) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1169 (0x2) and .absSeg1821 (0x2) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1821 (0x2) and .absSeg655 (0x3) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg2 (0x4) and .absSeg656 (0x4) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg656 (0x4) and .absSeg1170 (0x4) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1170 (0x4) and .absSeg1822 (0x4) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1822 (0x4) and .absSeg657 (0x5) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg3 (0x6) and .absSeg658 (0x6) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg658 (0x6) and .absSeg1171 (0x6) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1171 (0x6) and .absSeg1823 (0x6) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1823 (0x6) and .absSeg659 (0x7) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg4 (0x8) and .absSeg660 (0x8) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg660 (0x8) and .absSeg1172 (0x8) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1172 (0x8) and .absSeg1824 (0x8) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg5 (0x9) and .absSeg661 (0x9) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg661 (0x9) and .absSeg1173 (0x9) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1173 (0x9) and .absSeg1825 (0x9) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg6 (0xA) and .absSeg662 (0xA) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg662 (0xA) and .absSeg1174 (0xA) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1174 (0xA) and .absSeg1826 (0xA) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg7 (0xB) and .absSeg663 (0xB) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg663 (0xB) and .absSeg1175 (0xB) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1175 (0xB) and .absSeg1827 (0xB) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg8 (0xC) and .absSeg664 (0xC) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg664 (0xC) and .absSeg1176 (0xC) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1176 (0xC) and .absSeg1828 (0xC) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg9 (0xD) and .absSeg665 (0xD) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg665 (0xD) and .absSeg1177 (0xD) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1177 (0xD) and .absSeg1829 (0xD) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg10 (0x10) and .absSeg668 (0x10) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg668 (0x10) and .absSeg1178 (0x10) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1178 (0x10) and .absSeg1830 (0x10) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg11 (0x12) and .absSeg669 (0x12) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg669 (0x12) and .absSeg1179 (0x12) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1179 (0x12) and .absSeg1831 (0x12) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg12 (0x13) and .absSeg670 (0x13) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg670 (0x13) and .absSeg1180 (0x13) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1180 (0x13) and .absSeg1832 (0x13) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg13 (0x16) and .absSeg672 (0x16) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg672 (0x16) and .absSeg1181 (0x16) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1181 (0x16) and .absSeg1833 (0x16) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg14 (0x17) and .absSeg673 (0x17) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg673 (0x17) and .absSeg1182 (0x17) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg1182 (0x17) and .absSeg1834 (0x17) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING L1100: Segments .absSeg15 (0x1A) and .absSeg675 (0x1A) overlap&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;INFORMATION L2: Message overflow, skipping WARNING messages&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Before I added the linker option "-WmsgSw1100" these warnings were errors! As I don't like to see/get these warnings/errors everytime&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I compile my project, I would like to fix it, but I don't know how:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't change the software module which is including the other definition file and I want to use "my own" favorite register definition file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any way to get rid of these warnings (without turning this warning off)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2006 20:11:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/L1100-linker-errors-with-CodeWarrior-HC12-toolchain/m-p/137404#M1995</guid>
      <dc:creator>svenny29</dc:creator>
      <dc:date>2006-05-30T20:11:11Z</dc:date>
    </item>
    <item>
      <title>Re: L1100 linker errors with CodeWarrior HC12 toolchain</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/L1100-linker-errors-with-CodeWarrior-HC12-toolchain/m-p/137405#M1996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've seen this slew of errors when I use the CodeWarrior project wizard to build the HC12 version of OSEK. OSEK provides its own HC12 header information. Those files, along with the standard boiler-plate headers the CodeWarrior project provides, create redundant definitions. What you are seeing is the linker complaining of these redundant definitions.&lt;BR /&gt;&lt;BR /&gt;You're either going to have to live with the other software's header files, or carefully edit the CodeWarrior header file to include only the information that the other header files lack.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2006 20:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/L1100-linker-errors-with-CodeWarrior-HC12-toolchain/m-p/137405#M1996</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2006-05-30T20:52:59Z</dc:date>
    </item>
  </channel>
</rss>