<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: CW 11.1 Error - Error initializing Debug Database.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2013980#M16086</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243913"&gt;@kaspt&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post. Are you logging on Windows with Administrator right? &amp;nbsp;Could you please install the CodeWarrior under the default path?&lt;/P&gt;
&lt;P&gt;C:\Freescale\CW MCU v11.1&lt;/P&gt;
&lt;P&gt;Or you can also try the method in the following post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595042" target="_blank"&gt;Help with the "Debug Database Initialization" message? - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Download the "Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)" from Microsoft and repair the package that was installed with CW to see if it works.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Celeste&lt;BR /&gt;--------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct button. Thank you!&lt;BR /&gt;--------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 16 Dec 2024 02:03:56 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2024-12-16T02:03:56Z</dc:date>
    <item>
      <title>CW 11.1 Error - Error initializing Debug Database.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2013516#M16085</link>
      <description>&lt;P&gt;When opening a new empty workspace Code warrior dumps the error:&lt;/P&gt;&lt;P&gt;Error initializing Debug Database.&lt;/P&gt;&lt;P&gt;Could not load debug database. This is indication of an installation or configuration problem. Please contact customer support.&lt;/P&gt;&lt;P&gt;CodeWarrior for MCU &amp;nbsp;Version: 11.1 &amp;nbsp;Build Id:181224&lt;/P&gt;&lt;P&gt;There was allready a similar issue with a previes version.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-5-Error-quot-Debug-Database-Initialization-quot/m-p/257087" target="_blank"&gt;CW 10.5 Error - "Debug Database Initialization" - NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But there is no solution that works for me.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This&amp;nbsp;present’s me from debugging and flashing applications. Diagnostic report attached.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 09:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2013516#M16085</guid>
      <dc:creator>kaspt</dc:creator>
      <dc:date>2024-12-13T09:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: CW 11.1 Error - Error initializing Debug Database.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2013980#M16086</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243913"&gt;@kaspt&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post. Are you logging on Windows with Administrator right? &amp;nbsp;Could you please install the CodeWarrior under the default path?&lt;/P&gt;
&lt;P&gt;C:\Freescale\CW MCU v11.1&lt;/P&gt;
&lt;P&gt;Or you can also try the method in the following post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595042" target="_blank"&gt;Help with the "Debug Database Initialization" message? - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Download the "Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)" from Microsoft and repair the package that was installed with CW to see if it works.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Celeste&lt;BR /&gt;--------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct button. Thank you!&lt;BR /&gt;--------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 02:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2013980#M16086</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2024-12-16T02:03:56Z</dc:date>
    </item>
    <item>
      <title>Re: CW 11.1 Error - Error initializing Debug Database.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2017218#M16087</link>
      <description>&lt;P&gt;I installed code warrior under a different path (not the default one) now it works.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 12:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-11-1-Error-Error-initializing-Debug-Database/m-p/2017218#M16087</guid>
      <dc:creator>kaspt</dc:creator>
      <dc:date>2024-12-19T12:35:04Z</dc:date>
    </item>
  </channel>
</rss>