<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: v10.3 download</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/2002587#M16073</link>
    <description>&lt;P&gt;2024 is almost ending and there are still people who have to debug and add features on older products with Coldfire MCF5484 (&lt;A title="ColdFire® V4e Microcontroller with Ethernet, CAN and Encryption" href="https://www.nxp.com/products/MCF548X" target="_self"&gt;https://www.nxp.com/products/MCF548X&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;We use the P&amp;amp;E Multilink Debug Probe. In the current CodeWarrior IDE v11.1 it's not possible to connect to the controller.&lt;/P&gt;&lt;P&gt;Where can we get the last CodeWarrior IDE which is suitable for this?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Robert&lt;/P&gt;</description>
    <pubDate>Wed, 27 Nov 2024 07:23:45 GMT</pubDate>
    <dc:creator>R_Basta</dc:creator>
    <dc:date>2024-11-27T07:23:45Z</dc:date>
    <item>
      <title>v10.3 download</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/763242#M14578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone have a link to v10.3 for download.&amp;nbsp; I'm running into the debugger issues with later version, need to debug on Coldfire MCF5484 device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 15:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/763242#M14578</guid>
      <dc:creator>johnbils</dc:creator>
      <dc:date>2018-04-04T15:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: v10.3 download</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/763243#M14579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That version is no longer available on our website, I'm checking with the Software team to see if that version is available in one of our repositories.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 19:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/763243#M14579</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-04-09T19:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: v10.3 download</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/2002587#M16073</link>
      <description>&lt;P&gt;2024 is almost ending and there are still people who have to debug and add features on older products with Coldfire MCF5484 (&lt;A title="ColdFire® V4e Microcontroller with Ethernet, CAN and Encryption" href="https://www.nxp.com/products/MCF548X" target="_self"&gt;https://www.nxp.com/products/MCF548X&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;We use the P&amp;amp;E Multilink Debug Probe. In the current CodeWarrior IDE v11.1 it's not possible to connect to the controller.&lt;/P&gt;&lt;P&gt;Where can we get the last CodeWarrior IDE which is suitable for this?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Robert&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 07:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/v10-3-download/m-p/2002587#M16073</guid>
      <dc:creator>R_Basta</dc:creator>
      <dc:date>2024-11-27T07:23:45Z</dc:date>
    </item>
  </channel>
</rss>