<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S12 load a s19 trough sermon. in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12-load-a-s19-trough-sermon/m-p/1783694#M15977</link>
    <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to write a Windows application for load a s19 file in a S12 mcu using the regular serial monitor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I look for more information on how to send the data to the mcu.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where I can find the algorithm for initialize a firmware update and send data and write commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also timing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hard to understand with the bootloader description.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it more documents for the bootloader described in the AN2548 ?&lt;/P&gt;&lt;P&gt;I guess I understand most of the functionality.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The point I am struggling is what commands I have to send in which order with which amount of data for burn a single line of s2 record with page adress.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have successfully compiled the monitor and burned it in a dragonfly board for development propose and started to develop a application but don't have the way for burn the firmware trough serial for now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jan 2024 12:37:51 GMT</pubDate>
    <dc:creator>Yaban</dc:creator>
    <dc:date>2024-01-05T12:37:51Z</dc:date>
    <item>
      <title>S12 load a s19 trough sermon.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12-load-a-s19-trough-sermon/m-p/1783694#M15977</link>
      <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to write a Windows application for load a s19 file in a S12 mcu using the regular serial monitor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I look for more information on how to send the data to the mcu.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where I can find the algorithm for initialize a firmware update and send data and write commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also timing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hard to understand with the bootloader description.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it more documents for the bootloader described in the AN2548 ?&lt;/P&gt;&lt;P&gt;I guess I understand most of the functionality.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The point I am struggling is what commands I have to send in which order with which amount of data for burn a single line of s2 record with page adress.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have successfully compiled the monitor and burned it in a dragonfly board for development propose and started to develop a application but don't have the way for burn the firmware trough serial for now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 12:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12-load-a-s19-trough-sermon/m-p/1783694#M15977</guid>
      <dc:creator>Yaban</dc:creator>
      <dc:date>2024-01-05T12:37:51Z</dc:date>
    </item>
  </channel>
</rss>