<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックprogram data Flash using DSC Flash Programmer</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/program-data-Flash-using-DSC-Flash-Programmer/m-p/1399974#M15641</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Recently, I try to use Multilink Universal to download the data to the Data Flash of MC56F8345, I met below program even I used the same file which just generated by dumping Flash by DSC Flash programmer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fl::target -lc "MC56F8345_FLASH_LDM_PnE U-MultiLink"&lt;BR /&gt;fl::target -b 0x2fc00 0x400&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "MC56F8345_X_FLASH" -o "4kx16x1" -a 0x1000 0x1fff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM--3355.BIN" -t "Binary/Raw Format" -re off -oe off&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt;Beginning Operation ...&lt;BR /&gt;-------------------------&lt;BR /&gt;Nothing to erase. No sectors selected&lt;BR /&gt;Performing target initialization ...&lt;BR /&gt;Erase Command Succeeded.&lt;BR /&gt;cmdwin::fl::write&lt;BR /&gt;-------------------------&lt;BR /&gt;Flash Operation. ...&lt;BR /&gt;Programming ...&lt;BR /&gt;Programming warning. Can't program 8192 bytes to address 0x0 because this range isn't included in the selected modules!&lt;BR /&gt;Program Command Succeeded&lt;BR /&gt;Flash Operation. done&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM-3355.BIN" -t "Auto Detect" -re off -oe off&lt;BR /&gt;cmdwin::fl::verify&lt;BR /&gt;-------------------------&lt;BR /&gt;C:\Users\HardyCao\Desktop\SBD\Project\SAM\Software\firmware\ATM-3355.BIN&lt;BR /&gt;Flash Operation. ...&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Programming warning. Can't verify 8192 bytes to address 0x0 because this range isn't included in the selected modules!&lt;BR /&gt;Verify Command Succeeded&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jan 2022 06:28:49 GMT</pubDate>
    <dc:creator>HardyCao</dc:creator>
    <dc:date>2022-01-17T06:28:49Z</dc:date>
    <item>
      <title>program data Flash using DSC Flash Programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/program-data-Flash-using-DSC-Flash-Programmer/m-p/1399974#M15641</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Recently, I try to use Multilink Universal to download the data to the Data Flash of MC56F8345, I met below program even I used the same file which just generated by dumping Flash by DSC Flash programmer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fl::target -lc "MC56F8345_FLASH_LDM_PnE U-MultiLink"&lt;BR /&gt;fl::target -b 0x2fc00 0x400&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "MC56F8345_X_FLASH" -o "4kx16x1" -a 0x1000 0x1fff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM--3355.BIN" -t "Binary/Raw Format" -re off -oe off&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt;Beginning Operation ...&lt;BR /&gt;-------------------------&lt;BR /&gt;Nothing to erase. No sectors selected&lt;BR /&gt;Performing target initialization ...&lt;BR /&gt;Erase Command Succeeded.&lt;BR /&gt;cmdwin::fl::write&lt;BR /&gt;-------------------------&lt;BR /&gt;Flash Operation. ...&lt;BR /&gt;Programming ...&lt;BR /&gt;Programming warning. Can't program 8192 bytes to address 0x0 because this range isn't included in the selected modules!&lt;BR /&gt;Program Command Succeeded&lt;BR /&gt;Flash Operation. done&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM-3355.BIN" -t "Auto Detect" -re off -oe off&lt;BR /&gt;cmdwin::fl::verify&lt;BR /&gt;-------------------------&lt;BR /&gt;C:\Users\HardyCao\Desktop\SBD\Project\SAM\Software\firmware\ATM-3355.BIN&lt;BR /&gt;Flash Operation. ...&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Programming warning. Can't verify 8192 bytes to address 0x0 because this range isn't included in the selected modules!&lt;BR /&gt;Verify Command Succeeded&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 06:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/program-data-Flash-using-DSC-Flash-Programmer/m-p/1399974#M15641</guid>
      <dc:creator>HardyCao</dc:creator>
      <dc:date>2022-01-17T06:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: program data Flash using DSC Flash Programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/program-data-Flash-using-DSC-Flash-Programmer/m-p/1462807#M15686</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you use multilink Universal device to download code to MC56F8345 flash, I suppose that that you can use third party PROGDSC tools from the link, the tools is free of charge.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&amp;amp;productTab=5" target="_blank"&gt;https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&amp;amp;productTab=5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If your PC uses Win10 OS, I suppose that you can install the CodeWarrior for MCU ver11.x, and use the tools to download S-Record file to flash of MC56F8345.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 02:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/program-data-Flash-using-DSC-Flash-Programmer/m-p/1462807#M15686</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-05-24T02:21:45Z</dc:date>
    </item>
  </channel>
</rss>