<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: How to toggle one RGB LED after another with the SW2 and SW3 from frdmk64f?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-toggle-one-RGB-LED-after-another-with-the-SW2-and-SW3/m-p/1303727#M15567</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the gpio demo in SDK. The demo uses the button to control/toggle the LED&lt;/P&gt;
&lt;P&gt;SDK_2.9.0_FRDM-K64F\boards\frdmk64f\driver_examples\gpio\input_interrupt&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 07:57:48 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2021-07-07T07:57:48Z</dc:date>
    <item>
      <title>How to toggle one RGB LED after another with the SW2 and SW3 from frdmk64f?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-toggle-one-RGB-LED-after-another-with-the-SW2-and-SW3/m-p/1291669#M15551</link>
      <description>&lt;P&gt;Hi, I'm very new to this forum. So I apologize if this isn't the right thread or sub-thread. Basically, I'm experimenting and trying to learn new things with the Frdmk64f. I'm basically trying to get SW2 toggle one color LED and by pressing SW3 should toggle another color LED. And when both LED are ON, the LED will blend the two color.&lt;BR /&gt;Here's what I got so far:&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;BR /&gt;#include "board.h"&lt;BR /&gt;#include "peripherals.h"&lt;BR /&gt;#include "pin_mux.h"&lt;BR /&gt;#include "clock_config.h"&lt;BR /&gt;#include "MK64F12.h"&lt;BR /&gt;#include "fsl_debug_console.h"&lt;/P&gt;&lt;P&gt;void BOARD_SW2_IRQHANDLER(void) /*Interrupt Service Routine for SW2*/&lt;BR /&gt;{&lt;BR /&gt;uint32_t flags = GPIO_PortGetInterruptFlags(BOARD_SW2_GPIO); /*get triggered interrupt flag*/&lt;BR /&gt;GPIO_PortClearInterruptFlags(BOARD_SW2_GPIO, flags); /*clear triggered interrupt flag*/&lt;BR /&gt;LED_RED_ON(); /*turn ON RED LED*/&lt;BR /&gt;}&lt;BR /&gt;void BOARD_SW3_IRQHANDLER(void) /*Interrupt Service Routine for SW3*/&lt;BR /&gt;{&lt;BR /&gt;uint32_t flags = GPIO_PortGetInterruptFlags(BOARD_SW3_GPIO); /*get triggered interrupt flag*/&lt;BR /&gt;GPIO_PortClearInterruptFlags(BOARD_SW3_GPIO, flags); /*clear triggered interrupt flag*/&lt;BR /&gt;LED_RED_OFF(); /*turn OFF RED LED*/&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;int main(void) {&lt;/P&gt;&lt;P&gt;/* Init board hardware. */&lt;BR /&gt;BOARD_InitBootPins();&lt;BR /&gt;BOARD_InitBootClocks();&lt;BR /&gt;BOARD_InitBootPeripherals();&lt;BR /&gt;/* Init FSL debug console. */&lt;BR /&gt;BOARD_InitDebugConsole();&lt;/P&gt;&lt;P&gt;PRINTF("Hello World\n");&lt;/P&gt;&lt;P&gt;/* Force the counter to be placed into memory. */&lt;BR /&gt;volatile static int i = 0 ;&lt;BR /&gt;/* Enter an infinite loop, just incrementing a counter. */&lt;BR /&gt;while(1) {&lt;BR /&gt;i++ ;&lt;BR /&gt;/* 'Dummy' NOP to allow source level single stepping of&lt;BR /&gt;tight while() loop */&lt;BR /&gt;__asm volatile ("nop");&lt;BR /&gt;}&lt;BR /&gt;return 0 ;&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Sun, 13 Jun 2021 15:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-toggle-one-RGB-LED-after-another-with-the-SW2-and-SW3/m-p/1291669#M15551</guid>
      <dc:creator>paper</dc:creator>
      <dc:date>2021-06-13T15:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to toggle one RGB LED after another with the SW2 and SW3 from frdmk64f?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-toggle-one-RGB-LED-after-another-with-the-SW2-and-SW3/m-p/1303727#M15567</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the gpio demo in SDK. The demo uses the button to control/toggle the LED&lt;/P&gt;
&lt;P&gt;SDK_2.9.0_FRDM-K64F\boards\frdmk64f\driver_examples\gpio\input_interrupt&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 07:57:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-toggle-one-RGB-LED-after-another-with-the-SW2-and-SW3/m-p/1303727#M15567</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-07-07T07:57:48Z</dc:date>
    </item>
  </channel>
</rss>