<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Creating libraries</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Creating-libraries/m-p/1190384#M15511</link>
    <description>&lt;P&gt;Hi Jennie.&lt;/P&gt;&lt;P&gt;I am having problems following your instructions for creating a library: -&lt;/P&gt;&lt;P&gt;1. I created a new library project, but there is no "main.c" and there is a Debug folder, which is empty.&lt;/P&gt;&lt;P&gt;2. I have been using Windows on a MAC, using a virtual machine for about 10 years without any problems with CW but I do not have any function keys mapped, so what do I do instead of ALT+F7&lt;/P&gt;&lt;P&gt;3. Your library project was created with the name&amp;nbsp;mylib : MC9S08QG8_library, whereas my library project has the name mylib : Debug&lt;/P&gt;&lt;P&gt;In desperation I tried to edit and re-compile your file mylibrary.c, but nothing changed when ran your test project.&lt;/P&gt;&lt;P&gt;Finally, I have about 10 projects that use various members of the S08 family where approximately 50% of the code is common to all. Do I have to copy the .lib and .h files into each of them? This would be a big problem if or when I need to modify a library function. There would probably be about 12 functions in the library&lt;/P&gt;</description>
    <pubDate>Fri, 27 Nov 2020 17:53:21 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2020-11-27T17:53:21Z</dc:date>
    <item>
      <title>Creating libraries</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Creating-libraries/m-p/1190384#M15511</link>
      <description>&lt;P&gt;Hi Jennie.&lt;/P&gt;&lt;P&gt;I am having problems following your instructions for creating a library: -&lt;/P&gt;&lt;P&gt;1. I created a new library project, but there is no "main.c" and there is a Debug folder, which is empty.&lt;/P&gt;&lt;P&gt;2. I have been using Windows on a MAC, using a virtual machine for about 10 years without any problems with CW but I do not have any function keys mapped, so what do I do instead of ALT+F7&lt;/P&gt;&lt;P&gt;3. Your library project was created with the name&amp;nbsp;mylib : MC9S08QG8_library, whereas my library project has the name mylib : Debug&lt;/P&gt;&lt;P&gt;In desperation I tried to edit and re-compile your file mylibrary.c, but nothing changed when ran your test project.&lt;/P&gt;&lt;P&gt;Finally, I have about 10 projects that use various members of the S08 family where approximately 50% of the code is common to all. Do I have to copy the .lib and .h files into each of them? This would be a big problem if or when I need to modify a library function. There would probably be about 12 functions in the library&lt;/P&gt;</description>
      <pubDate>Fri, 27 Nov 2020 17:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Creating-libraries/m-p/1190384#M15511</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2020-11-27T17:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: Creating libraries</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Creating-libraries/m-p/1191983#M15513</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;I tested the sample code, I didn't see any issue. see attached video.&lt;/P&gt;
&lt;P&gt;you can change the name of "&lt;SPAN&gt;Debug&lt;/SPAN&gt;" based on your requirement. see video as well.&lt;/P&gt;
&lt;P&gt;For lib, make sure the extension is .lib&lt;/P&gt;
&lt;DIV id="tinyMceEditorZhangJennie_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV id="tinyMceEditorZhangJennie_1" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 04:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Creating-libraries/m-p/1191983#M15513</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-12-02T04:26:47Z</dc:date>
    </item>
  </channel>
</rss>