<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5644A GPIO-GPDO Error in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MPC5644A-GPIO-GPDO-Error/m-p/1135037#M15459</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I'm using mpc5644a. I have set the 124th pin as GPIO output pin. However, I have observed that the value assigned to register GPDO [124] is set in register GPDO [123]. At the same time, I observed that this happened from pin 101 to pin 145. (Address has been defined twice for GPDO [101].)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tgc-yilmaz_0-1599058462962.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124075iB8BEB75555A2118A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tgc-yilmaz_0-1599058462962.png" alt="tgc-yilmaz_0-1599058462962.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;tgc-yilmaz_0-1599058462962.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;NOTE: The same is true for GPDI[101]. However, no shift was observed in the GPDI[] registers.&lt;/P&gt;&lt;P&gt;What is the reason for this situation?&lt;/P&gt;&lt;P&gt;If there is an error, is there a published error record that describes this situation? Can you help with this?&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;Thanks in advance.&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Sep 2020 08:04:17 GMT</pubDate>
    <dc:creator>tgc-yilmaz</dc:creator>
    <dc:date>2020-09-03T08:04:17Z</dc:date>
    <item>
      <title>MPC5644A GPIO-GPDO Error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MPC5644A-GPIO-GPDO-Error/m-p/1135037#M15459</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I'm using mpc5644a. I have set the 124th pin as GPIO output pin. However, I have observed that the value assigned to register GPDO [124] is set in register GPDO [123]. At the same time, I observed that this happened from pin 101 to pin 145. (Address has been defined twice for GPDO [101].)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tgc-yilmaz_0-1599058462962.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124075iB8BEB75555A2118A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tgc-yilmaz_0-1599058462962.png" alt="tgc-yilmaz_0-1599058462962.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;tgc-yilmaz_0-1599058462962.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;NOTE: The same is true for GPDI[101]. However, no shift was observed in the GPDI[] registers.&lt;/P&gt;&lt;P&gt;What is the reason for this situation?&lt;/P&gt;&lt;P&gt;If there is an error, is there a published error record that describes this situation? Can you help with this?&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;Thanks in advance.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 08:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MPC5644A-GPIO-GPDO-Error/m-p/1135037#M15459</guid>
      <dc:creator>tgc-yilmaz</dc:creator>
      <dc:date>2020-09-03T08:04:17Z</dc:date>
    </item>
  </channel>
</rss>