<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: S12GA48MLF support in Codewarrior 5.2</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083388#M15439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112517i7F3EA528428B0B03/image-size/large?v=v2&amp;amp;px=999" title="USBDM_version.jpg" alt="USBDM_version.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 17:55:38 GMT</pubDate>
    <dc:creator>nkgavali1</dc:creator>
    <dc:date>2020-06-10T17:55:38Z</dc:date>
    <item>
      <title>S12GA48MLF support in Codewarrior 5.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083387#M15438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3 years before I used S12GA48MLF micro in Codewarrior 5.1. I used USBDM 4.12.1.80. That time I applied patch for PE for getting GA48 in codewarrior. But, now, I lost all data as my disk crashed and dont have back-up&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I would like to start the same board with same USBDM. I have downloaded USBDM current version &lt;SPAN&gt;4.12.1&lt;/SPAN&gt;.262 and codewarrior 5.1 special edition. I installed it and it has also installed codewarrior 5.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In&amp;nbsp;&lt;SPAN&gt;codewarrior 5.2, I can select the&amp;nbsp;S12GA48 microcontroller in the project. When I tried to debug it, it is not halted at any breakpoints&amp;nbsp;or interrupt. The error it is showing that the MCU ID 0x1C5 and not supported in HIwave debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I try to connect programmer over USBDM, it is showing chip ID F280 of G48. The image is attached here.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to know why it is happening? is there any change has made in CW5.2 or driver?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;NKG&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 17:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083387#M15438</guid>
      <dc:creator>nkgavali1</dc:creator>
      <dc:date>2020-06-10T17:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: S12GA48MLF support in Codewarrior 5.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083388#M15439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112517i7F3EA528428B0B03/image-size/large?v=v2&amp;amp;px=999" title="USBDM_version.jpg" alt="USBDM_version.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 17:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083388#M15439</guid>
      <dc:creator>nkgavali1</dc:creator>
      <dc:date>2020-06-10T17:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: S12GA48MLF support in Codewarrior 5.2</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083389#M15440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW5.2 only supports below interfaces:&lt;/P&gt;&lt;P&gt;USB ML 12 &lt;BR /&gt;USB Multilink Universal RevA-C&lt;BR /&gt;USB Multilink Universal FX RevA-B&lt;BR /&gt;Cyclone Pro (USB, Ethernet, Serial)&lt;BR /&gt;Cyclone Universal (USB, Ethernet, Serial)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Others are no longer supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 02:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/S12GA48MLF-support-in-Codewarrior-5-2/m-p/1083389#M15440</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-06-11T02:16:30Z</dc:date>
    </item>
  </channel>
</rss>