<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 The calculated CRC is incorrect</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/The-calculated-CRC-is-incorrect/m-p/1028513#M15363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using Codewarrior 11.1 to compile the program of the S12ZVMC256 chip. In the prm file, use the CHECKSUM command to calculate the CRC of the application code. The method used is METHOD_CRC8 (Figure 1). Unfortunately, the calculated CRC result is shown as B6 (Figure 2), which is incorrect. The correct CRC should be D5. What is the reason? The project I tested is shown in the attachment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Mar 2020 02:55:23 GMT</pubDate>
    <dc:creator>林联伟</dc:creator>
    <dc:date>2020-03-16T02:55:23Z</dc:date>
    <item>
      <title>The calculated CRC is incorrect</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/The-calculated-CRC-is-incorrect/m-p/1028513#M15363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using Codewarrior 11.1 to compile the program of the S12ZVMC256 chip. In the prm file, use the CHECKSUM command to calculate the CRC of the application code. The method used is METHOD_CRC8 (Figure 1). Unfortunately, the calculated CRC result is shown as B6 (Figure 2), which is incorrect. The correct CRC should be D5. What is the reason? The project I tested is shown in the attachment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2020 02:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/The-calculated-CRC-is-incorrect/m-p/1028513#M15363</guid>
      <dc:creator>林联伟</dc:creator>
      <dc:date>2020-03-16T02:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: The calculated CRC is incorrect</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/The-calculated-CRC-is-incorrect/m-p/1028514#M15364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The METHOD_CRC8 algorithm used in CodeWarrior can be find in attached checksum files.&lt;/P&gt;&lt;P&gt;Please refer attached files to generate CRC8 method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 07:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/The-calculated-CRC-is-incorrect/m-p/1028514#M15364</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-03-26T07:36:15Z</dc:date>
    </item>
  </channel>
</rss>