<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックLoad the program in batch for S08</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Load-the-program-in-batch-for-S08/m-p/1011236#M15303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team!&lt;/P&gt;&lt;P&gt;I am using MCU MC9S08PT for our product&lt;BR /&gt;My problem now is that when the mass production (Average 500,000pcs / year), now workers have to load the program one by one (Using CodeWarrior and Multilink Universal FX), it takes too much time and does not reach production capacity.&lt;BR /&gt;Is there a better way for us? For example, program loader 1 for many products&lt;BR /&gt;Note: We change the design constantly for different products so do not pre-load firmware from the supplier&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2020 09:25:44 GMT</pubDate>
    <dc:creator>lelam</dc:creator>
    <dc:date>2020-02-25T09:25:44Z</dc:date>
    <item>
      <title>Load the program in batch for S08</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Load-the-program-in-batch-for-S08/m-p/1011236#M15303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team!&lt;/P&gt;&lt;P&gt;I am using MCU MC9S08PT for our product&lt;BR /&gt;My problem now is that when the mass production (Average 500,000pcs / year), now workers have to load the program one by one (Using CodeWarrior and Multilink Universal FX), it takes too much time and does not reach production capacity.&lt;BR /&gt;Is there a better way for us? For example, program loader 1 for many products&lt;BR /&gt;Note: We change the design constantly for different products so do not pre-load firmware from the supplier&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2020 09:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Load-the-program-in-batch-for-S08/m-p/1011236#M15303</guid>
      <dc:creator>lelam</dc:creator>
      <dc:date>2020-02-25T09:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: Load the program in batch for S08</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Load-the-program-in-batch-for-S08/m-p/1011237#M15304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Le,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;An option would be to use &lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320167&amp;amp;productTab=1"&gt;Cyclone-FX&lt;/A&gt; for production programming. Programming may be launched by a single button press without a host PC or automatically from a PC via the automated control SDK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, please check the Flash File to Target feature of Codewarrior. You can find more information in&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=CWCFUG&amp;amp;location=null"&gt;CodeWarrior Development Studio Common Features Guide&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 21:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Load-the-program-in-batch-for-S08/m-p/1011237#M15304</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-03-02T21:04:59Z</dc:date>
    </item>
  </channel>
</rss>