<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックError when using interprocedural analysis at program level</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-when-using-interprocedural-analysis-at-program-level/m-p/993387#M15287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am writing code for the MPC5645S architecture using Codewarrior MCU V10.6 with General Update V1.0.0.&lt;BR /&gt;Previously, the code was compiled and linked via command line with option '-ipa file' which did not make any problems.&lt;BR /&gt;Now I want to use the interprocedural analysis&amp;nbsp;at program level ('-ipa program'), but when trying to link the optimized files the following error message appears:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;### mwldeppc.exe Driver Error:&lt;BR /&gt;# License check failed: No such feature exists.&lt;BR /&gt;# Feature: Win32_Plugins_Link_PPC&lt;BR /&gt;# License path: C:\Freescale\CW MCU v10.6\MCU\Bin\..\license.dat;&lt;BR /&gt;# FLEXnet Licensing error:-5,357&lt;BR /&gt;# For further information, refer to the FLEXnet Licensing documentation,&lt;BR /&gt;# available at "www.macrovision.com".&lt;/P&gt;&lt;P&gt;Errors caused tool to abort.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;### mwcceppc.exe Driver Error:&lt;BR /&gt;# linker 'C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools\mwldeppc.exe' returned with exit code 1&lt;/P&gt;&lt;P&gt;Errors caused tool to abort.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB dongle is connected to my PC, else it would not link the code because it exceeds the code size limit.&lt;BR /&gt;I searched for the feature 'Win32_Plugins_Link_PPC' in the list of available licenses that I could activate on the nxp website, but I did not find anything related.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How can I get the interprocedural analysis work at program level?&lt;BR /&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Feb 2020 10:38:36 GMT</pubDate>
    <dc:creator>andreasschönman</dc:creator>
    <dc:date>2020-02-06T10:38:36Z</dc:date>
    <item>
      <title>Error when using interprocedural analysis at program level</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-when-using-interprocedural-analysis-at-program-level/m-p/993387#M15287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am writing code for the MPC5645S architecture using Codewarrior MCU V10.6 with General Update V1.0.0.&lt;BR /&gt;Previously, the code was compiled and linked via command line with option '-ipa file' which did not make any problems.&lt;BR /&gt;Now I want to use the interprocedural analysis&amp;nbsp;at program level ('-ipa program'), but when trying to link the optimized files the following error message appears:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;### mwldeppc.exe Driver Error:&lt;BR /&gt;# License check failed: No such feature exists.&lt;BR /&gt;# Feature: Win32_Plugins_Link_PPC&lt;BR /&gt;# License path: C:\Freescale\CW MCU v10.6\MCU\Bin\..\license.dat;&lt;BR /&gt;# FLEXnet Licensing error:-5,357&lt;BR /&gt;# For further information, refer to the FLEXnet Licensing documentation,&lt;BR /&gt;# available at "www.macrovision.com".&lt;/P&gt;&lt;P&gt;Errors caused tool to abort.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;### mwcceppc.exe Driver Error:&lt;BR /&gt;# linker 'C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools\mwldeppc.exe' returned with exit code 1&lt;/P&gt;&lt;P&gt;Errors caused tool to abort.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB dongle is connected to my PC, else it would not link the code because it exceeds the code size limit.&lt;BR /&gt;I searched for the feature 'Win32_Plugins_Link_PPC' in the list of available licenses that I could activate on the nxp website, but I did not find anything related.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How can I get the interprocedural analysis work at program level?&lt;BR /&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2020 10:38:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-when-using-interprocedural-analysis-at-program-level/m-p/993387#M15287</guid>
      <dc:creator>andreasschönman</dc:creator>
      <dc:date>2020-02-06T10:38:36Z</dc:date>
    </item>
  </channel>
</rss>