<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Exception is received when using PIT &amp; FreeRTOS</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-PIT-FreeRTOS/m-p/975116#M15262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using SDK RTM 3.0 with S32DS for the MPC5748G. &lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I opened the example&amp;nbsp; freertos_mpc5748g&amp;nbsp; project, from the supplied examples, the code runs as expected.&lt;BR /&gt;However, when I add a pit interrupt component and try to call the interrupt callback the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;BR /&gt;If I use the same pit interrupt code without FreeRTOS, all works fine as well. &lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Has anyone seen this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Dec 2019 15:37:10 GMT</pubDate>
    <dc:creator>dazhou0503</dc:creator>
    <dc:date>2019-12-12T15:37:10Z</dc:date>
    <item>
      <title>Exception is received when using PIT &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-PIT-FreeRTOS/m-p/975116#M15262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using SDK RTM 3.0 with S32DS for the MPC5748G. &lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I opened the example&amp;nbsp; freertos_mpc5748g&amp;nbsp; project, from the supplied examples, the code runs as expected.&lt;BR /&gt;However, when I add a pit interrupt component and try to call the interrupt callback the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;BR /&gt;If I use the same pit interrupt code without FreeRTOS, all works fine as well. &lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Has anyone seen this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 15:37:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-PIT-FreeRTOS/m-p/975116#M15262</guid>
      <dc:creator>dazhou0503</dc:creator>
      <dc:date>2019-12-12T15:37:10Z</dc:date>
    </item>
    <item>
      <title>Re: Exception is received when using PIT &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-PIT-FreeRTOS/m-p/975117#M15263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This sound to me like you haven't PIT interrupt priority higher than uSDHC interrupt.&lt;/P&gt;&lt;P&gt;Have in mind that OS is serving interrupts instead your INTC handler in non OS example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 09:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-PIT-FreeRTOS/m-p/975117#M15263</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-12-13T09:18:23Z</dc:date>
    </item>
  </channel>
</rss>