<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Use MULTILINK UNIVERSAL FX With FreeMASTER in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929216#M15155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;is&amp;nbsp;your problem resolved?&amp;nbsp;Before using the Multilink Universal, please make sure a correct HCS08-compatible firmware is loaded to it. The Multilink firmware is updated any time you use&amp;nbsp;it to download or debug an application from CodeWarrior environment.&amp;nbsp;P&amp;amp;E Micro should also provide a firmware update/switch tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FreeMASTER itself is not able to update the Multilink firmware, but it should work correctly with the Multilink and S08 family after it is updated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Dec 2019 14:16:14 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2019-12-03T14:16:14Z</dc:date>
    <item>
      <title>Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929211#M15150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I use CW to develop Touch for the S08PT family.&lt;BR /&gt;Is there any way to use FreeMASTER without using the COM port.&lt;BR /&gt;I am having a MULTILINK UNIVERSAL FX&amp;nbsp;, can use it ?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2019 07:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929211#M15150</guid>
      <dc:creator>lelam</dc:creator>
      <dc:date>2019-09-30T07:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929212#M15151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;The Multilink Universal FX does support FreeMASTER for the S08PT family. I would suggest downloading the newest version, FreeMASTER 2.0, so that you will have all the updated device support.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;If you are unable to connect, there is a chance that some of your files need to be updated. If this is the case, contact PEmicro and we will be more than happy to help with this.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Steve&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 13:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929212#M15151</guid>
      <dc:creator>steven_mcgrath</dc:creator>
      <dc:date>2019-10-02T13:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929213#M15152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr.Steve,&lt;/P&gt;&lt;P&gt;I am using FreeMASTER V 2.5.13.0, it is the latest.&lt;BR /&gt;Maybe I need to contact PEmicro, hope they can help us?&lt;BR /&gt;Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 03:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929213#M15152</guid>
      <dc:creator>lelam</dc:creator>
      <dc:date>2019-10-03T03:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929214#M15153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes PEmicro will be able to provide you with the latest files that should get you up and running with the newest version of FreeMASTER. I would suggest visiting the homepage &lt;A href="http://www.pemicro.com"&gt;www.pemicro.com&lt;/A&gt;&amp;nbsp;and going to the "Support" tab. Here you can setup a Support Request and a representative will be able to provide you with the necessary files once that is done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 15:21:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929214#M15153</guid>
      <dc:creator>steven_mcgrath</dc:creator>
      <dc:date>2019-10-03T15:21:09Z</dc:date>
    </item>
    <item>
      <title>Re: Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929215#M15154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Yes,&amp;nbsp;I have created a ticket code 28109, and waiting.&lt;BR /&gt;Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 02:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929215#M15154</guid>
      <dc:creator>lelam</dc:creator>
      <dc:date>2019-10-07T02:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: Use MULTILINK UNIVERSAL FX With FreeMASTER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929216#M15155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;is&amp;nbsp;your problem resolved?&amp;nbsp;Before using the Multilink Universal, please make sure a correct HCS08-compatible firmware is loaded to it. The Multilink firmware is updated any time you use&amp;nbsp;it to download or debug an application from CodeWarrior environment.&amp;nbsp;P&amp;amp;E Micro should also provide a firmware update/switch tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FreeMASTER itself is not able to update the Multilink firmware, but it should work correctly with the Multilink and S08 family after it is updated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 14:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Use-MULTILINK-UNIVERSAL-FX-With-FreeMASTER/m-p/929216#M15155</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2019-12-03T14:16:14Z</dc:date>
    </item>
  </channel>
</rss>