<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Exception is received when using can_pal &amp; FreeRTOS</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876635#M15010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a similar problem.Using SDK RTM 3.0 with S32DS for the MPC5748G.&lt;/P&gt;&lt;P&gt;I opened the example freertos_mpc5748g project, from the supplied examples, the code runs as expected.&lt;BR /&gt;However, when I add a pit component and try to call the pit interrupt callback the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Dec 2019 15:42:20 GMT</pubDate>
    <dc:creator>dazhou0503</dc:creator>
    <dc:date>2019-12-12T15:42:20Z</dc:date>
    <item>
      <title>Exception is received when using can_pal &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876633#M15008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using SDK RTM 2.0 with S32DS for the MPC5748G.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I opened a new FreeRTOS project, from the supplied examples, the code runs as expected.&lt;BR /&gt;However, when I add a CAN_pal component and try to call the CAN_send the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;BR /&gt;If I use the same CAN_pal code without FreeRTOS, all works fine as well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone seen this issue?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 15:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876633#M15008</guid>
      <dc:creator>alon_becker</dc:creator>
      <dc:date>2019-03-07T15:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: Exception is received when using can_pal &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876634#M15009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please share your project? Most probably, it will be necessary to ask SDK development team directly, and they will need your project to check, what is not correctly configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 07:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876634#M15009</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2019-03-14T07:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: Exception is received when using can_pal &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876635#M15010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a similar problem.Using SDK RTM 3.0 with S32DS for the MPC5748G.&lt;/P&gt;&lt;P&gt;I opened the example freertos_mpc5748g project, from the supplied examples, the code runs as expected.&lt;BR /&gt;However, when I add a pit component and try to call the pit interrupt callback the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 15:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/876635#M15010</guid>
      <dc:creator>dazhou0503</dc:creator>
      <dc:date>2019-12-12T15:42:20Z</dc:date>
    </item>
    <item>
      <title>Re: Exception is received when using can_pal &amp; FreeRTOS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/1320789#M15594</link>
      <description>&lt;P&gt;I am also facing same issue. After adding ADC, EEPROM, to USB demo code, whenever I am executing&amp;nbsp;&lt;SPAN&gt;the core jumps to uSDHC_DriverIRQHandler although this module is not active.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 05:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Exception-is-received-when-using-can-pal-FreeRTOS/m-p/1320789#M15594</guid>
      <dc:creator>priya_p</dc:creator>
      <dc:date>2021-08-10T05:23:01Z</dc:date>
    </item>
  </channel>
</rss>