<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RN8 memory usage view, how many FLASH &amp; RAM do I use (with Codewarrior 11)? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864122#M14979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a S9S08RNA8 µC and I use Codewarrior 11 for my application software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seach now for a way to see how many memory (flash and/or RAM) my µC is using. I don't men the memory view while debugging with the codewarrior. This is working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean a way to see in percent or in kB how high my memory usage is. Is there another programm instead of CW11 which can do it?&lt;/P&gt;&lt;P&gt;Any other suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2019 09:40:35 GMT</pubDate>
    <dc:creator>sebe</dc:creator>
    <dc:date>2019-01-09T09:40:35Z</dc:date>
    <item>
      <title>RN8 memory usage view, how many FLASH &amp; RAM do I use (with Codewarrior 11)?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864122#M14979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a S9S08RNA8 µC and I use Codewarrior 11 for my application software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seach now for a way to see how many memory (flash and/or RAM) my µC is using. I don't men the memory view while debugging with the codewarrior. This is working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean a way to see in percent or in kB how high my memory usage is. Is there another programm instead of CW11 which can do it?&lt;/P&gt;&lt;P&gt;Any other suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 09:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864122#M14979</guid>
      <dc:creator>sebe</dc:creator>
      <dc:date>2019-01-09T09:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: RN8 memory usage view, how many FLASH &amp; RAM do I use (with Codewarrior 11)?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864123#M14980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastian Felix,&lt;/P&gt;&lt;P&gt;CodeWarrior can generate a map file after a SUCCESSFUL build.&lt;/P&gt;&lt;P&gt;In map file, it summarize the used memory sizes based on the section type. see below demonstration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76627i24234807E4AB1255/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 09:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864123#M14980</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-01-10T09:16:15Z</dc:date>
    </item>
    <item>
      <title>Re: RN8 memory usage view, how many FLASH &amp; RAM do I use (with Codewarrior 11)?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864124#M14981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, thanks. This helps me.&lt;/P&gt;&lt;P&gt;I checked it with my softwares and it looks okay for me. READ_ONLY is flash+EEPROM and READ_WRITE looks like the RAM.&lt;/P&gt;&lt;P&gt;NO_INIT, is something what will not be initialized. Somehow all my projects have the same NO_INIT size, 225. I think this is µC specific, which will be different If I take a larger or another type of µC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perfect, thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 07:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864124#M14981</guid>
      <dc:creator>sebe</dc:creator>
      <dc:date>2019-01-11T07:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: RN8 memory usage view, how many FLASH &amp; RAM do I use (with Codewarrior 11)?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864125#M14982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Jan 2019 10:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/RN8-memory-usage-view-how-many-FLASH-RAM-do-I-use-with/m-p/864125#M14982</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-01-13T10:36:50Z</dc:date>
    </item>
  </channel>
</rss>