<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Interfacing two MC9S12XEP100 using CAN MAX3050 interface</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843350#M14870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.&lt;/P&gt;&lt;P&gt;Is there any sample code available for the same as per your protocol standards ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Dec 2018 04:09:39 GMT</pubDate>
    <dc:creator>harshal_pawar</dc:creator>
    <dc:date>2018-12-07T04:09:39Z</dc:date>
    <item>
      <title>Interfacing two MC9S12XEP100 using CAN MAX3050 interface</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843350#M14870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.&lt;/P&gt;&lt;P&gt;Is there any sample code available for the same as per your protocol standards ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 04:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843350#M14870</guid>
      <dc:creator>harshal_pawar</dc:creator>
      <dc:date>2018-12-07T04:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing two MC9S12XEP100 using CAN MAX3050 interface</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843351#M14871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Harshal,&lt;/P&gt;&lt;P&gt;I recommend you refer AN3034 for CAN design&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3034.pdf" title="https://www.nxp.com/docs/en/application-note/AN3034.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3034.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=AN3034SW&amp;amp;location=null" title="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=AN3034SW&amp;amp;location=null"&gt;Software for AN3034&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 06:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843351#M14871</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-12-11T06:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing two MC9S12XEP100 using CAN MAX3050 interface</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843352#M14872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 04:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843352#M14872</guid>
      <dc:creator>harshal_pawar</dc:creator>
      <dc:date>2018-12-12T04:02:25Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing two MC9S12XEP100 using CAN MAX3050 interface</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843353#M14873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 05:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Interfacing-two-MC9S12XEP100-using-CAN-MAX3050-interface/m-p/843353#M14873</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-12-12T05:47:17Z</dc:date>
    </item>
  </channel>
</rss>