<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックCodeWarrior 8- &amp; 16-bit tools: Flash programmer problem</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-8-16-bit-tools-Flash-programmer-problem/m-p/124993#M148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;To help you find solutions to problems that have already been solved, we have posted this message. It contains an entire topic ported from a separate forum. The original message and all replies are in this single message.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;AKULKARNI308&lt;BR /&gt;Posted: Jun 13, 2005 - 08:18 AM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;i have made a board using MCF5407, 4Mbytes of SDRAM and 2Mbytes of Flash. I have customised the TRD project to suit my board. When I click the option of Flash Programming-&amp;gt;Connect.. it connects. But when I try any of the below options like Blank Check, Program Flash, Erase etc I get the following error :&lt;BR /&gt;"CFP:Target Blank Check has timed out. Please check target board and connection settings and try again"&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;this error is for blank check.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;No matter what i do in the TRD file I have this error.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can someone help me on this issue ?&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;STRONG&gt;mw_uahmad&lt;BR /&gt;Posted: Jun 17, 2005 - 03:47 PM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Our flash programmer seems to support the following flash configuration: part: am29pl160cb and has 1M x 16 x 1 of flash. Yours is 2mb which could be causing problems. I don't believe we have a configuration for a 2mb flash size. You can alternatively use the CFlasher from the freescale website and see if that works.&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;STRONG&gt;AKULKARNI308&lt;BR /&gt;Posted: Jun 22, 2005 - 01:17 AM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The flash I am using is 1Mx16 bit which is 2mb. Also, I have tried the P&amp;amp;E flash programmer and it works fine. So, basically the hardware is working fine.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The problem is with the configuration of Mwerks programming utility.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The flash I am using is M29W160DB-90N1.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What is the correct procedure to configure it in the source code?&lt;BR /&gt;No matter what i do I get the error (as stated in the last email)&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Also, whenever I install P&amp;amp;E utility for coldfire my Mwerks IDE does not work .. It gives me some memory error .. i am using Windows 98. Is that a problem ?&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mw_uahmad&lt;BR /&gt;Posted: Jun 23, 2005 - 06:34 PM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The flash part you have listed does not seem to be a supported part in both Coldfire 4.x and 5.x. However in 5.x you do have the ability to add a flash device in the Flash programmer's settings. There is not a way to do that in 4.x. If you look in the personality files listings in the Flash programmer panel, your flash part is not listed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Jan 2006 02:37:42 GMT</pubDate>
    <dc:creator>marc_paquette</dc:creator>
    <dc:date>2006-01-28T02:37:42Z</dc:date>
    <item>
      <title>CodeWarrior 8- &amp; 16-bit tools: Flash programmer problem</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-8-16-bit-tools-Flash-programmer-problem/m-p/124993#M148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;To help you find solutions to problems that have already been solved, we have posted this message. It contains an entire topic ported from a separate forum. The original message and all replies are in this single message.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;AKULKARNI308&lt;BR /&gt;Posted: Jun 13, 2005 - 08:18 AM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;i have made a board using MCF5407, 4Mbytes of SDRAM and 2Mbytes of Flash. I have customised the TRD project to suit my board. When I click the option of Flash Programming-&amp;gt;Connect.. it connects. But when I try any of the below options like Blank Check, Program Flash, Erase etc I get the following error :&lt;BR /&gt;"CFP:Target Blank Check has timed out. Please check target board and connection settings and try again"&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;this error is for blank check.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;No matter what i do in the TRD file I have this error.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can someone help me on this issue ?&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;STRONG&gt;mw_uahmad&lt;BR /&gt;Posted: Jun 17, 2005 - 03:47 PM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Our flash programmer seems to support the following flash configuration: part: am29pl160cb and has 1M x 16 x 1 of flash. Yours is 2mb which could be causing problems. I don't believe we have a configuration for a 2mb flash size. You can alternatively use the CFlasher from the freescale website and see if that works.&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;STRONG&gt;AKULKARNI308&lt;BR /&gt;Posted: Jun 22, 2005 - 01:17 AM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The flash I am using is 1Mx16 bit which is 2mb. Also, I have tried the P&amp;amp;E flash programmer and it works fine. So, basically the hardware is working fine.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The problem is with the configuration of Mwerks programming utility.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The flash I am using is M29W160DB-90N1.&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What is the correct procedure to configure it in the source code?&lt;BR /&gt;No matter what i do I get the error (as stated in the last email)&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Also, whenever I install P&amp;amp;E utility for coldfire my Mwerks IDE does not work .. It gives me some memory error .. i am using Windows 98. Is that a problem ?&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mw_uahmad&lt;BR /&gt;Posted: Jun 23, 2005 - 06:34 PM&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The flash part you have listed does not seem to be a supported part in both Coldfire 4.x and 5.x. However in 5.x you do have the ability to add a flash device in the Flash programmer's settings. There is not a way to do that in 4.x. If you look in the personality files listings in the Flash programmer panel, your flash part is not listed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Jan 2006 02:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-8-16-bit-tools-Flash-programmer-problem/m-p/124993#M148</guid>
      <dc:creator>marc_paquette</dc:creator>
      <dc:date>2006-01-28T02:37:42Z</dc:date>
    </item>
  </channel>
</rss>