<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 target request failed failed to set breakpoint</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/target-request-failed-failed-to-set-breakpoint/m-p/806880#M14759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running Codewarrior for MCU version 11.0.1 build 180609 with an MC9S08GT16a.&amp;nbsp;&amp;nbsp;My project is a relocatable assembly project.&amp;nbsp; When I try to run the debugger, I get a pop-up saying "Error stopping at main.&amp;nbsp; Reason: Target request failed: Failed to set breakpoint.&amp;nbsp; Continue?"&amp;nbsp; If I click "Yes" the debugger starts and seems to run normally.&amp;nbsp; But what is the source of the annoying pop-up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previous threads on this problem have been no help.&amp;nbsp; When I created a new project with the same source files, I got the same pop-up.&amp;nbsp; And the "Strip symbolic information" box is not checked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Nov 2018 19:54:31 GMT</pubDate>
    <dc:creator>Mockingbird</dc:creator>
    <dc:date>2018-11-27T19:54:31Z</dc:date>
    <item>
      <title>target request failed failed to set breakpoint</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/target-request-failed-failed-to-set-breakpoint/m-p/806880#M14759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running Codewarrior for MCU version 11.0.1 build 180609 with an MC9S08GT16a.&amp;nbsp;&amp;nbsp;My project is a relocatable assembly project.&amp;nbsp; When I try to run the debugger, I get a pop-up saying "Error stopping at main.&amp;nbsp; Reason: Target request failed: Failed to set breakpoint.&amp;nbsp; Continue?"&amp;nbsp; If I click "Yes" the debugger starts and seems to run normally.&amp;nbsp; But what is the source of the annoying pop-up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previous threads on this problem have been no help.&amp;nbsp; When I created a new project with the same source files, I got the same pop-up.&amp;nbsp; And the "Strip symbolic information" box is not checked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 19:54:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/target-request-failed-failed-to-set-breakpoint/m-p/806880#M14759</guid>
      <dc:creator>Mockingbird</dc:creator>
      <dc:date>2018-11-27T19:54:31Z</dc:date>
    </item>
    <item>
      <title>Re: target request failed failed to set breakpoint</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/target-request-failed-failed-to-set-breakpoint/m-p/806881#M14760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Timothy Phillips&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any problem if you test your code in full chip simulation mode?&lt;/P&gt;&lt;P&gt;Is this problem in any relocatable assembly code?&lt;/P&gt;&lt;P&gt;if this is not a common issue, please upload your demo project, we can check it directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 06:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/target-request-failed-failed-to-set-breakpoint/m-p/806881#M14760</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-11-29T06:40:04Z</dc:date>
    </item>
  </channel>
</rss>