<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックOptimize compiler for code size</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Optimize-compiler-for-code-size/m-p/793943#M14724</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I amusing CW 10.7 with a S08SH4 processor. Is there an option to configure the compiler to minimise code size? Also, what is the approximate difference in code size between the Debug and Release configurations?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Sep 2018 09:29:06 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2018-09-05T09:29:06Z</dc:date>
    <item>
      <title>Optimize compiler for code size</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Optimize-compiler-for-code-size/m-p/793943#M14724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I amusing CW 10.7 with a S08SH4 processor. Is there an option to configure the compiler to minimise code size? Also, what is the approximate difference in code size between the Debug and Release configurations?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 09:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Optimize-compiler-for-code-size/m-p/793943#M14724</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2018-09-05T09:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize compiler for code size</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Optimize-compiler-for-code-size/m-p/793944#M14725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="285141" data-username="juliancox" href="https://community.nxp.com/people/juliancox"&gt;Julian Cox ,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;- Yes, you can reduce code size through Properties-&amp;gt; C/C++ Build -&amp;gt;Setting -&amp;gt; .... as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68289iBA89AEE63E5369F0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;You can find the detail description in "MCU_HCS08_compiler"-&amp;gt; 7.2.3.1.58 -O(-Os, -Ot): Main Optimization Target .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;- What about the debug and release of your project ? they can configure by ourself , you can also check the defferent setting in Properties, or you can send your project to me .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;Hope it helps,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-acclaim-count="0" data-acclaim-type="like" data-bullet="true" data-can-apply="true" data-type="medium"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 13:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Optimize-compiler-for-code-size/m-p/793944#M14725</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-09-05T13:57:27Z</dc:date>
    </item>
  </channel>
</rss>