<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: CW11 Indexing issue</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786658#M14678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gian,&lt;/P&gt;&lt;P&gt;can you try disabling the heuristics check box as shown in &lt;A class="link-titled" href="https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/" title="https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/"&gt;Fixing the Eclipse Index | MCU on Eclipse&lt;/A&gt;?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 18:08:53 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2018-08-14T18:08:53Z</dc:date>
    <item>
      <title>CW11 Indexing issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786657#M14677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Today, starting CW11.0 on a project I have been working on for a few week,s in the Progress window appeared "C/C++Indexer", Indexing : 2/3 sources, 0 headers: parsing handle_function.c(/terminator_pa_21062018/Sources/Functions) and nothing else is happening.....any suggestion? The IDE would not close at all after this message shows up......&lt;/P&gt;&lt;P&gt;Quite often I also have problems during debugging in displaying the variables: instead of showing all variables declared it repeats the same one or few ones several times.....what is the reason for it?&lt;/P&gt;&lt;P&gt;Gian Paolo Adamati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 16:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786657#M14677</guid>
      <dc:creator>gpadam</dc:creator>
      <dc:date>2018-08-14T16:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: CW11 Indexing issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786658#M14678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gian,&lt;/P&gt;&lt;P&gt;can you try disabling the heuristics check box as shown in &lt;A class="link-titled" href="https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/" title="https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/"&gt;Fixing the Eclipse Index | MCU on Eclipse&lt;/A&gt;?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 18:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786658#M14678</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-08-14T18:08:53Z</dc:date>
    </item>
    <item>
      <title>Re: CW11 Indexing issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786659#M14679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;heuristic check box is already disabled in my project ( I never modified this setting so I think it's the default for CW11.0).&lt;/P&gt;&lt;P&gt;The indexer is in an infinite loop and there is no way I can kill the process.....something definitely messed up the entire workspace, I had to move the current project to a new one and then it worked... not a pleasant event!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea about the variables displaying problem during debugging?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, another issue: every in a while and in debugging, during firmware download I have an "error 51 message" mostly regarding the EEPROM area (CRC block error). My eeprom area&amp;nbsp; (256 bytes) is fully declared as&amp;nbsp; a "const unsigned char" array, I double checked it with a S19 viewer and all the bytes are declared: any idea of why is doing it? I tend to exclude hardware problems but it is not nice to debug&amp;nbsp; some code or data when you are not sure if it is stored as it should in eeprom or flash......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 13:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW11-Indexing-issue/m-p/786659#M14679</guid>
      <dc:creator>gpadam</dc:creator>
      <dc:date>2018-08-16T13:51:12Z</dc:date>
    </item>
  </channel>
</rss>