<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 No .s19 file</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785459#M14667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This appears to be a recurring problem for me. Everything is fine until, for no apparent reason, CW 11(and CW 10.7)&amp;nbsp;for S08 will not generate a S19 file. If i enable the option in the debug settings I can get a Sx file but I need a abs.s19 file to use with my Cyclone. I have checked the burner.bbl file and the makefile and there appears to be no difference between a project that creates the S19 file and a project that does not. If I disable the s-record option in the build settings I get nothing.&lt;/P&gt;&lt;P&gt;As an alternative to throwing my computer off a very high building, can I use the burner in a stand-alone mode to create a s19 file.&lt;/P&gt;&lt;P&gt;By the way, the only solution in the past has been to create a new project and cut and paste the source files.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2018 11:44:21 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2018-10-12T11:44:21Z</dc:date>
    <item>
      <title>No .s19 file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785459#M14667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This appears to be a recurring problem for me. Everything is fine until, for no apparent reason, CW 11(and CW 10.7)&amp;nbsp;for S08 will not generate a S19 file. If i enable the option in the debug settings I can get a Sx file but I need a abs.s19 file to use with my Cyclone. I have checked the burner.bbl file and the makefile and there appears to be no difference between a project that creates the S19 file and a project that does not. If I disable the s-record option in the build settings I get nothing.&lt;/P&gt;&lt;P&gt;As an alternative to throwing my computer off a very high building, can I use the burner in a stand-alone mode to create a s19 file.&lt;/P&gt;&lt;P&gt;By the way, the only solution in the past has been to create a new project and cut and paste the source files.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 11:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785459#M14667</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2018-10-12T11:44:21Z</dc:date>
    </item>
    <item>
      <title>Re: No .s19 file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785460#M14668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julian,&lt;/P&gt;&lt;P&gt;maybe this is your problem:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2013/06/12/traps-and-pitfalls-no-hexbins19-file-created-with-gnu/" title="https://mcuoneclipse.com/2013/06/12/traps-and-pitfalls-no-hexbins19-file-created-with-gnu/"&gt;Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 18:20:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785460#M14668</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-10-12T18:20:14Z</dc:date>
    </item>
    <item>
      <title>Re: No .s19 file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785461#M14669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Using the Burner (in GUI mode) gave me a quick solution - so thanks. However, you may be interested in the following: -&lt;/P&gt;&lt;P&gt;Once I confirmed that the s19 file was correct I repeated the exercise with the output file destination in the Flash folder of the project (where it would have been if it was working correctly). I then closed and re-opened CW and the s19 file was there. I then made a change to the source code and carried out a Build of the project. Surprise!!!!!!! The last line in the Console window showed that the Burner had be called and a new updated s19 file had be generated.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 08:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785461#M14669</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2018-10-16T08:52:53Z</dc:date>
    </item>
    <item>
      <title>Re: No .s19 file</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785462#M14670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julien,&lt;/P&gt;&lt;P&gt;if that file exist on disk, it might be that the Eclipse view did not show it? You might need to do a 'Refresh' (F5) (context menu on that folder).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other thing you could check is that if your refresh policy is referring your project (and not something else), see &lt;A class="jivelink11" href="https://mcuoneclipse.com/2015/06/06/eclipse-project-refresh-policy-broken-incremental-build-with-external-make/" title="https://mcuoneclipse.com/2015/06/06/eclipse-project-refresh-policy-broken-incremental-build-with-external-make/"&gt;https://mcuoneclipse.com/2015/06/06/eclipse-project-refresh-policy-broken-incremental-build-with-external-make/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 09:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/No-s19-file/m-p/785462#M14670</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-10-16T09:17:34Z</dc:date>
    </item>
  </channel>
</rss>