<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic flash write and read/ in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/779783#M14640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir/ms.&lt;/P&gt;&lt;P&gt;   I have made a program in codewarrior 10.7,the cpu is mc56f84789. In PE, I have met two problems, they are follows.&lt;/P&gt;&lt;P&gt;  1.  I have added a flash module in my program,but I can not  read or write the flash correctly, can you give me an example that how I read or write the flash? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;  2. I have added eFlexPWM module, there is a fault in my program when the PWM fault pin is high level. If there is a fault, sometimes enter the fault interrupt,sometimes does not enter the fault interrupt,  how can I  set the fault pin  to enter the fault interrupt ? or which options  can I set to enter the fault interrupt? can you give me an example? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;chunhua guo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Feb 2018 10:59:04 GMT</pubDate>
    <dc:creator>guochunhua</dc:creator>
    <dc:date>2018-02-03T10:59:04Z</dc:date>
    <item>
      <title>flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/779783#M14640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir/ms.&lt;/P&gt;&lt;P&gt;   I have made a program in codewarrior 10.7,the cpu is mc56f84789. In PE, I have met two problems, they are follows.&lt;/P&gt;&lt;P&gt;  1.  I have added a flash module in my program,but I can not  read or write the flash correctly, can you give me an example that how I read or write the flash? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;  2. I have added eFlexPWM module, there is a fault in my program when the PWM fault pin is high level. If there is a fault, sometimes enter the fault interrupt,sometimes does not enter the fault interrupt,  how can I  set the fault pin  to enter the fault interrupt ? or which options  can I set to enter the fault interrupt? can you give me an example? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;chunhua guo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Feb 2018 10:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/779783#M14640</guid>
      <dc:creator>guochunhua</dc:creator>
      <dc:date>2018-02-03T10:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/779784#M14641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chunhua,&lt;/P&gt;&lt;P&gt;This is a duplicate question of&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/469202"&gt;https://community.nxp.com/thread/469202&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have support engineer already contacted you via that link.&lt;/P&gt;&lt;P&gt;Please have a look, if that's not clear, please contact the support engineer with reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Jennie Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2018 02:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/779784#M14641</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-02-11T02:45:45Z</dc:date>
    </item>
  </channel>
</rss>