<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: flash write and read/</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773905#M14602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Guo,&lt;/P&gt;&lt;P&gt;Regarding the flash writting/reading, I have only the code based on PE, I attach it, hope it can help you.&lt;/P&gt;&lt;P&gt;Regarding the fault of eFlexPWM, the interrupt index 77 is the eFlexPWMA fault vector, the FLVL bits in PWMA_FCTRLn set the fault logic, the FIE bits set the faultx pin interrupt enable, the PWMA_FAULT bits in INTC_IPR8 set the interrupt priority.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Feb 2018 09:34:39 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-02-09T09:34:39Z</dc:date>
    <item>
      <title>flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773904#M14601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir/ms.&lt;/P&gt;&lt;P&gt;   I have made a program in codewarrior 10.7,the cpu is mc56f84789. In PE, I have met two problems, they are follows.&lt;/P&gt;&lt;P&gt;  1.  I have added a flash module in my program,but I can not  read or write the flash correctly, can you give me an example that how I read or write the flash? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;  2. I have added eFlexPWM module, there is a fault in my program when the PWM fault pin is high level. If there is a fault, sometimes enter the fault interrupt,sometimes does not enter the fault interrupt,  how can I  set the fault pin  to enter the fault interrupt ? or which options  can I set to enter the fault interrupt? can you give me an example? It is wonderful if you can give me a video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;chunhua guo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jan 2018 10:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773904#M14601</guid>
      <dc:creator>guochunhua</dc:creator>
      <dc:date>2018-01-31T10:54:54Z</dc:date>
    </item>
    <item>
      <title>Re: flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773905#M14602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Guo,&lt;/P&gt;&lt;P&gt;Regarding the flash writting/reading, I have only the code based on PE, I attach it, hope it can help you.&lt;/P&gt;&lt;P&gt;Regarding the fault of eFlexPWM, the interrupt index 77 is the eFlexPWMA fault vector, the FLVL bits in PWMA_FCTRLn set the fault logic, the FIE bits set the faultx pin interrupt enable, the PWMA_FAULT bits in INTC_IPR8 set the interrupt priority.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 09:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773905#M14602</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-02-09T09:34:39Z</dc:date>
    </item>
    <item>
      <title>Re: flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773906#M14603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rong&lt;/P&gt;&lt;P&gt;Thank you for your help,regarding the flash writting/reading, I am sorry I can not find the code based on PE that you attached, can you attach it again?thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Chunhua Guo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2018 11:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773906#M14603</guid>
      <dc:creator>guochunhua</dc:creator>
      <dc:date>2018-02-12T11:50:13Z</dc:date>
    </item>
    <item>
      <title>Re: flash write and read/</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773907#M14604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Chunhua,&lt;/P&gt;&lt;P&gt;I attach it here.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 01:57:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/flash-write-and-read/m-p/773907#M14604</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-02-13T01:57:48Z</dc:date>
    </item>
  </channel>
</rss>