<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: USBDM 4.12.1.30 ARM Programmer Issue</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBDM-4-12-1-30-ARM-Programmer-Issue/m-p/765522#M14590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="243606" data-username="diegovalerio" href="https://community.nxp.com/people/diegovalerio"&gt;Diego Valerio&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Does your project includes the code like printf to console , or other debug code ?&lt;/P&gt;&lt;P&gt;If yes, when flash it to chip , the project can't work well.&lt;/P&gt;&lt;P&gt;So could you please first test a simple project , like only a gpio (LED)&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Mar 2018 09:53:18 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2018-03-19T09:53:18Z</dc:date>
    <item>
      <title>USBDM 4.12.1.30 ARM Programmer Issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBDM-4-12-1-30-ARM-Programmer-Issue/m-p/765521#M14589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everybody.&lt;/P&gt;&lt;P&gt;I have some issues using the&amp;nbsp;USBDM 4.12.1.30 ARM Programmer.&lt;/P&gt;&lt;P&gt;I am working with a MKE02Z64M2 chip, and I am trying to program its Flash with the ARM Programmer, but I have communication errors when I introduce my programmed device in my system.&lt;/P&gt;&lt;P&gt;I generate the .s19 file with CW 10.6 following the next steps:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1. I enabled the option to Create Flash Image, with the Output format srec.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2. I compiled the program. I have the ProjName.hex file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;3. I copied the .hex file in the Computer Desktop and renamed it as ProjName.s19.&lt;/P&gt;&lt;P&gt;Then, with USBDM&amp;nbsp;&lt;SPAN&gt;4.12.1.30 ARM Programmer, I loaded the .s19 file. I selected the Device and Clicked Detect Chip.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In security I checked Image and in programming Erase Mode "Erase All" is selected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Then, I clicked Program Flash. It has no errors.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I introduce the device in my system, the communication gets wrong.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As when I debug in CodeWarrior, I can specify the Trim Options, ant it does not generate any trouble with the communication.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28793iBED12EB944F792AF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28903i4D1F7B52FE4C9A7B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think this is something that generates the trouble with my UART communication. In the USBDM ARM Programmer, I can't specify those values:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29002iE805943FD0B29F86/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The program loads correctly in the device, but when it tries to establish serial communication through its UART port, a lot of communication error occurs, but when I compiled it with CodeWarrior through a PEMicro Debbuger, the serial communication works fine. Hope I made my point clear.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could somebody help me with this? I need to be able to load .s19 files to my ARM devices with no errors like this one.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Diego.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 17:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBDM-4-12-1-30-ARM-Programmer-Issue/m-p/765521#M14589</guid>
      <dc:creator>diegovalerio</dc:creator>
      <dc:date>2018-03-16T17:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.12.1.30 ARM Programmer Issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBDM-4-12-1-30-ARM-Programmer-Issue/m-p/765522#M14590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="243606" data-username="diegovalerio" href="https://community.nxp.com/people/diegovalerio"&gt;Diego Valerio&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Does your project includes the code like printf to console , or other debug code ?&lt;/P&gt;&lt;P&gt;If yes, when flash it to chip , the project can't work well.&lt;/P&gt;&lt;P&gt;So could you please first test a simple project , like only a gpio (LED)&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 09:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USBDM-4-12-1-30-ARM-Programmer-Issue/m-p/765522#M14590</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-19T09:53:18Z</dc:date>
    </item>
  </channel>
</rss>