<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックCodeWarrior 5.1 Dflash Program</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-5-1-Dflash-Program/m-p/759140#M14534</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I defined a constant with a default value in the dflash of the software.But when I use BDM to program&amp;nbsp;the software to the MC9S12P128, I find that the dflash area of the defined data is not the default value I set, but all is 0xFF. I ues the CW 5.1 .But when I change to CW4.7, I also use the BDM flash method to see that the dflash area is the correct default value.&amp;nbsp;Why is there such a difference between CW5.1 and CW4.7? How can I use CW5.1 to program&amp;nbsp;dflash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2018 06:00:20 GMT</pubDate>
    <dc:creator>283230333</dc:creator>
    <dc:date>2018-04-03T06:00:20Z</dc:date>
    <item>
      <title>CodeWarrior 5.1 Dflash Program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-5-1-Dflash-Program/m-p/759140#M14534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I defined a constant with a default value in the dflash of the software.But when I use BDM to program&amp;nbsp;the software to the MC9S12P128, I find that the dflash area of the defined data is not the default value I set, but all is 0xFF. I ues the CW 5.1 .But when I change to CW4.7, I also use the BDM flash method to see that the dflash area is the correct default value.&amp;nbsp;Why is there such a difference between CW5.1 and CW4.7? How can I use CW5.1 to program&amp;nbsp;dflash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 06:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-5-1-Dflash-Program/m-p/759140#M14534</guid>
      <dc:creator>283230333</dc:creator>
      <dc:date>2018-04-03T06:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 5.1 Dflash Program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-5-1-Dflash-Program/m-p/759141#M14535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for contacting us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I couldn’t reproduce your problem. Can you please send me your demo code that runs under CW4.7 and CW5.1? I will check it directly from my side. Please mention which memory address you monitored.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 07:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-5-1-Dflash-Program/m-p/759141#M14535</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-04-04T07:45:20Z</dc:date>
    </item>
  </channel>
</rss>