<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Crashing Flash programmer</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Crashing-Flash-programmer/m-p/743046#M14421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to flash my MPC5604P via CW 10.7.&lt;/P&gt;&lt;P&gt;So i open the Flash programmer and create a new Connection. When it comes to selecting the Connection type i can choose between "GDI Generic" and "P&amp;amp;E Power PC Multilink\Multilink Universal\Cyclone Max\OSJTAG". I need the second one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After i choose it, CW will load for some seconds until it finally Chrashes. It will not Crash when i choose GDI Generic.&lt;/P&gt;&lt;P&gt;unfortunately i can't find any error log to look further into the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea whats wrong there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ps.:&lt;/P&gt;&lt;P&gt;I use Windows 10 Pro 64 Bit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Apr 2018 12:43:23 GMT</pubDate>
    <dc:creator>jlange</dc:creator>
    <dc:date>2018-04-18T12:43:23Z</dc:date>
    <item>
      <title>Crashing Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Crashing-Flash-programmer/m-p/743046#M14421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to flash my MPC5604P via CW 10.7.&lt;/P&gt;&lt;P&gt;So i open the Flash programmer and create a new Connection. When it comes to selecting the Connection type i can choose between "GDI Generic" and "P&amp;amp;E Power PC Multilink\Multilink Universal\Cyclone Max\OSJTAG". I need the second one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After i choose it, CW will load for some seconds until it finally Chrashes. It will not Crash when i choose GDI Generic.&lt;/P&gt;&lt;P&gt;unfortunately i can't find any error log to look further into the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea whats wrong there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ps.:&lt;/P&gt;&lt;P&gt;I use Windows 10 Pro 64 Bit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 12:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Crashing-Flash-programmer/m-p/743046#M14421</guid>
      <dc:creator>jlange</dc:creator>
      <dc:date>2018-04-18T12:43:23Z</dc:date>
    </item>
  </channel>
</rss>