<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: .cfg documentation</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739653#M14397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've seen that note (or something like it) before.&amp;nbsp; Trouble is there is no description of the commands / statements to be used in the .cfg and .mem files (searching returns no hits).&amp;nbsp; These files seem to be important if not essential when using CodeWarrior to get going with a new ColdFire-based board, so surely they must be documented somewhere?&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using PCBs created in-house, with external flash, etc. that does not match any of the eval boards, so I need to create specific cfg &amp;amp; mem files, and therefore want proper documentation for them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Nov 2017 09:48:20 GMT</pubDate>
    <dc:creator>gilesrobinson</dc:creator>
    <dc:date>2017-11-03T09:48:20Z</dc:date>
    <item>
      <title>.cfg documentation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739651#M14395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I feel I must be missing the obvious, but where is the documentation for the Initialization and Memory scripts for debugging?&lt;/P&gt;&lt;P&gt;For a ColdFire project I have ${ProjDirPath}/Project_Settings/Debugger/MCF5484.cfg and MCF5484.mem which I think need editing for the particular PCB.&amp;nbsp; Using a P&amp;amp;Emicro Multilink, I can connect and step (looking at the PC register), but can't read back the memory correctly.&amp;nbsp; I could guess at editing the settings for CS0 etc, but would like a proper reference guide.&lt;/P&gt;&lt;P&gt;So, where is the contents of these two files documented?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 14:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739651#M14395</guid>
      <dc:creator>gilesrobinson</dc:creator>
      <dc:date>2017-11-01T14:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: .cfg documentation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739652#M14396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Glies,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend you to take a look to the following application note for more information:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://cache.nxp.com/docs/en/application-note/AN3389.pdf" title="https://cache.nxp.com/docs/en/application-note/AN3389.pdf"&gt;https://cache.nxp.com/docs/en/application-note/AN3389.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 21:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739652#M14396</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-11-02T21:07:46Z</dc:date>
    </item>
    <item>
      <title>Re: .cfg documentation</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739653#M14397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've seen that note (or something like it) before.&amp;nbsp; Trouble is there is no description of the commands / statements to be used in the .cfg and .mem files (searching returns no hits).&amp;nbsp; These files seem to be important if not essential when using CodeWarrior to get going with a new ColdFire-based board, so surely they must be documented somewhere?&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using PCBs created in-house, with external flash, etc. that does not match any of the eval boards, so I need to create specific cfg &amp;amp; mem files, and therefore want proper documentation for them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 09:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/cfg-documentation/m-p/739653#M14397</guid>
      <dc:creator>gilesrobinson</dc:creator>
      <dc:date>2017-11-03T09:48:20Z</dc:date>
    </item>
  </channel>
</rss>