<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is BDM must to flash code to coldfire MCF51CN128cgt in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731879#M14329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I am using code warrior 10.2 for development. I am taking help of Application Note AN3906 for implementing a serial to ethernet bridge. I have also downloaded the software for AN3906 and imported it into code warrior as a project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whenever I try to build the project, I get an error as in the attached screenshot&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16523i887BB62B12D1B1E5/image-size/large?v=v2&amp;amp;px=999" title="Screenshot from 2018-01-18 14_27_57.png" alt="Screenshot from 2018-01-18 14_27_57.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The highlighted line reads as follows.&lt;/P&gt;&lt;P&gt;Libs/mcf51cn128_c.obj: /usr/local/Freescale/CodeWarrior_MCU_10.2/eclipse/C::/Program\ Files/Freescale/CW\ MCU\ v10.1/MCU/ColdFire_Support/Derivatives/device/src/mcf51cn128.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know here there is a conflict between windows and linux paths. But how to change the settings so the project only takes a linux path.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the readme.txt with the application note states that the sw is compiled for CW 10.1 , and I am using 10.2 so will this work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Awaiting your response eagerly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;SK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jan 2018 09:03:19 GMT</pubDate>
    <dc:creator>sanketk</dc:creator>
    <dc:date>2018-01-18T09:03:19Z</dc:date>
    <item>
      <title>Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731875#M14325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a newbie to coldfire devices. I am currently using MCF51CN128cgt coldfire V1 core for ethernet development.&lt;/P&gt;&lt;P&gt;Can we flash program the core using serial flash programming technique or it is necessary to use BDM multilink.&lt;/P&gt;&lt;P&gt;Also any hints on getting started with development for MCF51CN devices like which development tools to use are&lt;/P&gt;&lt;P&gt;appreciable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hoping to get the answers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;SK&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 06:25:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731875#M14325</guid>
      <dc:creator>sanketk</dc:creator>
      <dc:date>2018-01-17T06:25:56Z</dc:date>
    </item>
    <item>
      <title>Re: Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731876#M14326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SK,&lt;/P&gt;&lt;P&gt;BDM interface is necessary to develop, debug and program ColdFire V1 chip.&lt;/P&gt;&lt;P&gt;if you use NXP demo board, there is a BDM debug interface integrated on board, thus you don't need purchase a BDM emulator separately.&lt;/P&gt;&lt;P&gt;If you develop a customized Coldfire v1 board, you need have a BDM emulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User can also develop a bootloader, for example serial bootloader to program board. but BDM emulator is still needed to program bootloader into board first.&lt;/P&gt;&lt;P&gt;Is this clear for you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 07:50:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731876#M14326</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-01-17T07:50:00Z</dc:date>
    </item>
    <item>
      <title>Re: Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731877#M14327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You for the prompt answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes it is clear to me now. I have some few more queries related to development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1: What IDE do I&amp;nbsp;have to use for development.&lt;/P&gt;&lt;P&gt;2: Since I am using Linux OS, how should I set up the development environment on linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 08:42:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731877#M14327</guid>
      <dc:creator>sanketk</dc:creator>
      <dc:date>2018-01-17T08:42:28Z</dc:date>
    </item>
    <item>
      <title>Re: Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731878#M14328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SK.&lt;/P&gt;&lt;P&gt;We have CW v11 works for Coldfire v1. but there is only windows version variable.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-qorivva-56xx-rs08-s08-s12z-v11.0:CW-MCU10?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-qorivva-56xx-rs08-s08-s12z-v11.0:CW-MCU10?tab=Design_Tools_Tab"&gt;CodeWarrior for Microcontrollers-Eclipse IDE|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 08:40:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731878#M14328</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-01-18T08:40:10Z</dc:date>
    </item>
    <item>
      <title>Re: Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731879#M14329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I am using code warrior 10.2 for development. I am taking help of Application Note AN3906 for implementing a serial to ethernet bridge. I have also downloaded the software for AN3906 and imported it into code warrior as a project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whenever I try to build the project, I get an error as in the attached screenshot&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16523i887BB62B12D1B1E5/image-size/large?v=v2&amp;amp;px=999" title="Screenshot from 2018-01-18 14_27_57.png" alt="Screenshot from 2018-01-18 14_27_57.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The highlighted line reads as follows.&lt;/P&gt;&lt;P&gt;Libs/mcf51cn128_c.obj: /usr/local/Freescale/CodeWarrior_MCU_10.2/eclipse/C::/Program\ Files/Freescale/CW\ MCU\ v10.1/MCU/ColdFire_Support/Derivatives/device/src/mcf51cn128.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know here there is a conflict between windows and linux paths. But how to change the settings so the project only takes a linux path.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the readme.txt with the application note states that the sw is compiled for CW 10.1 , and I am using 10.2 so will this work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Awaiting your response eagerly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;SK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 09:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731879#M14329</guid>
      <dc:creator>sanketk</dc:creator>
      <dc:date>2018-01-18T09:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Is BDM must to flash code to coldfire MCF51CN128cgt</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731880#M14330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the demo code with AN3906 is for CW0.2 windows version.&lt;/P&gt;&lt;P&gt;to import a windows project to linux's, I know some CW10.2 linux version user do it by create a new project then add the files one by one.&lt;/P&gt;&lt;P&gt;Please note, CW10.2 linux is an intermediate version. we no longer recommend.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jennie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 09:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-BDM-must-to-flash-code-to-coldfire-MCF51CN128cgt/m-p/731880#M14330</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-01-24T09:22:27Z</dc:date>
    </item>
  </channel>
</rss>