<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックIs it possible to run multiple Debug sessions in Codewarrior Eclipse?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714653#M14194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior for MCU&lt;BR /&gt; Version: 10.6&lt;BR /&gt; Build Id:140329&lt;/P&gt;&lt;P&gt;Targeting&amp;nbsp;two 56800E processors.&lt;/P&gt;&lt;P&gt;Connecting to both via a USB tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our set up is that we have two identical processors on the same PCB that communicate with each other. I would like to have a debug session running on each, in case I would like to break on certain communication events.&lt;/P&gt;&lt;P&gt;I have two USB Tap probes. I have set it up so that&amp;nbsp;one project targets one USB Tap and the other project targeting the other Tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This works fine if I run one debug session at a time. They properly target the right USB tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I try to run both debug sessions at the same time, the second one I start throws the error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error launching [ProjectName] ldm external memory&lt;BR /&gt;CCSProtocolPlugin : CW found a living connection on CCS. It should be closed in order to connect again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've done some poking around and internet searches and have been unable to figure out if there is something I need to change, or if this is just not possible, but have come up empty. Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Sep 2017 13:17:49 GMT</pubDate>
    <dc:creator>Charlie</dc:creator>
    <dc:date>2017-09-27T13:17:49Z</dc:date>
    <item>
      <title>Is it possible to run multiple Debug sessions in Codewarrior Eclipse?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714653#M14194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior for MCU&lt;BR /&gt; Version: 10.6&lt;BR /&gt; Build Id:140329&lt;/P&gt;&lt;P&gt;Targeting&amp;nbsp;two 56800E processors.&lt;/P&gt;&lt;P&gt;Connecting to both via a USB tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our set up is that we have two identical processors on the same PCB that communicate with each other. I would like to have a debug session running on each, in case I would like to break on certain communication events.&lt;/P&gt;&lt;P&gt;I have two USB Tap probes. I have set it up so that&amp;nbsp;one project targets one USB Tap and the other project targeting the other Tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This works fine if I run one debug session at a time. They properly target the right USB tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I try to run both debug sessions at the same time, the second one I start throws the error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error launching [ProjectName] ldm external memory&lt;BR /&gt;CCSProtocolPlugin : CW found a living connection on CCS. It should be closed in order to connect again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've done some poking around and internet searches and have been unable to figure out if there is something I need to change, or if this is just not possible, but have come up empty. Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 13:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714653#M14194</guid>
      <dc:creator>Charlie</dc:creator>
      <dc:date>2017-09-27T13:17:49Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to run multiple Debug sessions in Codewarrior Eclipse?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714654#M14195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Charles,&lt;/P&gt;&lt;P&gt;We can't debug Multiple board with USB TAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 08:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714654#M14195</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-09-29T08:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to run multiple Debug sessions in Codewarrior Eclipse?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714655#M14196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Disappointing, but thanks for the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nice to know I'm not an idiot who couldn't figure it out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 15:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-it-possible-to-run-multiple-Debug-sessions-in-Codewarrior/m-p/714655#M14196</guid>
      <dc:creator>Charlie</dc:creator>
      <dc:date>2017-10-02T15:52:52Z</dc:date>
    </item>
  </channel>
</rss>