<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Hello. MPC5674F Link Command File (LCF) is being created. I want to enter unique information in the LCF. Is there a way to declare a symbol for unique information in the MPC5674F LCF and enter its symbol value?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-MPC5674F-Link-Command-File-LCF-is-being-created-I-want-to/m-p/706562#M14156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would suggest you submit a private case for this question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please detail what result you expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Oct 2017 05:22:45 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2017-10-30T05:22:45Z</dc:date>
    <item>
      <title>Hello. MPC5674F Link Command File (LCF) is being created. I want to enter unique information in the LCF. Is there a way to declare a symbol for unique information in the MPC5674F LCF and enter its symbol value?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-MPC5674F-Link-Command-File-LCF-is-being-created-I-want-to/m-p/706561#M14155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FLASH: 0x00000000 - 0x0003FFFFF */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Fixed location required for RCHW and program entry point*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; resetvector:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x00000000,&amp;nbsp;&amp;nbsp; len = 0x00000008&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Contains initializations from __ppc_eabi_init.c,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Should be 4K since the hardware automatically creates a default TLB entry&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; from the start of the entry point specified in RCHW.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; init:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x00000010,&amp;nbsp;&amp;nbsp; len = 0x00000FF0 /* ~4K */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* ~63K gap required to align the exception handlers.*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Contains interrupt branch tables for both core and INTC module&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; and the ISR handlers code. Note, the gap is required since the vector&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; base address field of core IVPR is defined within the range [0:15], the&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTC branch tables must be loaded at an address aligned to 64K boundary.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; exception_handlers: org = 0x00010000,&amp;nbsp;&amp;nbsp; len = 0x0020000 /* 128K */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Space allocated for user code and device initialization.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM Image address should be set with the start address of this&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; segment in order to instruct the runtime to initialize the&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; static variables. All the section above are ignored for this action. &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please see -romaddr linker option.*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; internal_flash:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x00030000,&amp;nbsp;&amp;nbsp; len = 0x003D0000 /* 3904K */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* SRAM: 0x40000000 - 0x4003FFFF */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; internal_ram:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x40000000,&amp;nbsp;&amp;nbsp; len = 0x00030000 /* 192KB */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; heap&amp;nbsp; :&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x40030000,&amp;nbsp;&amp;nbsp; len = 0x00008000 /* 32KB Heap start location */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; stack :&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; org = 0x40038000,&amp;nbsp;&amp;nbsp; len = 0x00008000 /* 32KB Start location for Stack */&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* ROM&amp;nbsp;SW ID */&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; rom_sw_id:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;org = 0x40035000,&amp;nbsp;&amp;nbsp; len = 0x0000000D&lt;/STRONG&gt;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SECTIONS&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;GROUP : {&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; /* I want to fill the value of symbol */&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;} &amp;gt; rom_sw_id&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 14:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-MPC5674F-Link-Command-File-LCF-is-being-created-I-want-to/m-p/706561#M14155</guid>
      <dc:creator>choonharyu</dc:creator>
      <dc:date>2017-10-13T14:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Hello. MPC5674F Link Command File (LCF) is being created. I want to enter unique information in the LCF. Is there a way to declare a symbol for unique information in the MPC5674F LCF and enter its symbol value?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-MPC5674F-Link-Command-File-LCF-is-being-created-I-want-to/m-p/706562#M14156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would suggest you submit a private case for this question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please detail what result you expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 05:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Hello-MPC5674F-Link-Command-File-LCF-is-being-created-I-want-to/m-p/706562#M14156</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-10-30T05:22:45Z</dc:date>
    </item>
  </channel>
</rss>