<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 anyway to stop erasing data flash?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/anyway-to-stop-erasing-data-flash/m-p/701077#M14125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using Code Warrior for MCU 10.6.4, DSP56F8357, P&amp;amp;E U-MultiLink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application uses internal Data Flash as EEProm to store user settings. This works well, and I can read, write, and erase segments no problem.&lt;/P&gt;&lt;P&gt;To free up data flash for my uses, in the linker.cmd file I have moved all the constant data from x flash to p flash, and this also works fine. At startup my constants get moved from p flash to x ram as intended. The linker map file shows that x flash is empty, so this leaves the entire x flash for my uses - which is what I wanted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is a problem that every time I download new code into the processor, the entire data flash gets erased automatically by code warrior somewhere. This wipes out my user's settings of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anywhere I can instruct code warrior or p&amp;amp;e to stop erasing data flash by default?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Oct 2017 20:30:37 GMT</pubDate>
    <dc:creator>skaiser</dc:creator>
    <dc:date>2017-10-09T20:30:37Z</dc:date>
    <item>
      <title>anyway to stop erasing data flash?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/anyway-to-stop-erasing-data-flash/m-p/701077#M14125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using Code Warrior for MCU 10.6.4, DSP56F8357, P&amp;amp;E U-MultiLink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application uses internal Data Flash as EEProm to store user settings. This works well, and I can read, write, and erase segments no problem.&lt;/P&gt;&lt;P&gt;To free up data flash for my uses, in the linker.cmd file I have moved all the constant data from x flash to p flash, and this also works fine. At startup my constants get moved from p flash to x ram as intended. The linker map file shows that x flash is empty, so this leaves the entire x flash for my uses - which is what I wanted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is a problem that every time I download new code into the processor, the entire data flash gets erased automatically by code warrior somewhere. This wipes out my user's settings of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anywhere I can instruct code warrior or p&amp;amp;e to stop erasing data flash by default?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 20:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/anyway-to-stop-erasing-data-flash/m-p/701077#M14125</guid>
      <dc:creator>skaiser</dc:creator>
      <dc:date>2017-10-09T20:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: anyway to stop erasing data flash?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/anyway-to-stop-erasing-data-flash/m-p/701078#M14126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;see &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/07/13/preserving-memory-ranges-with-eclipse-and-pe-gdb-server/" title="https://mcuoneclipse.com/2014/07/13/preserving-memory-ranges-with-eclipse-and-pe-gdb-server/"&gt;Preserving Memory Ranges with Eclipse and P&amp;amp;E GDB Server | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 03:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/anyway-to-stop-erasing-data-flash/m-p/701078#M14126</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-10-10T03:41:54Z</dc:date>
    </item>
  </channel>
</rss>