<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What does production use to program boards? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-production-use-to-program-boards/m-p/661208#M13866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using CW 10.6 with MQX to build projects for a K60 ARM. &amp;nbsp;I have a license and can debug and flash projects no problem using a PE micro Multilink Universal. So I thought I could generate .s19 files and have production use a unlicensed version of Codewarrior to flash boards. The flash programmer is easy to use. &amp;nbsp;I've tried two computers and get errors on both. &amp;nbsp;I attached one of the errors. &amp;nbsp;Is there a better way? &amp;nbsp;Is the license the issue? &amp;nbsp;What can get rid of this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 16:45:32 GMT</pubDate>
    <dc:creator>c_dawg</dc:creator>
    <dc:date>2017-02-22T16:45:32Z</dc:date>
    <item>
      <title>What does production use to program boards?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-production-use-to-program-boards/m-p/661208#M13866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using CW 10.6 with MQX to build projects for a K60 ARM. &amp;nbsp;I have a license and can debug and flash projects no problem using a PE micro Multilink Universal. So I thought I could generate .s19 files and have production use a unlicensed version of Codewarrior to flash boards. The flash programmer is easy to use. &amp;nbsp;I've tried two computers and get errors on both. &amp;nbsp;I attached one of the errors. &amp;nbsp;Is there a better way? &amp;nbsp;Is the license the issue? &amp;nbsp;What can get rid of this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 16:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-production-use-to-program-boards/m-p/661208#M13866</guid>
      <dc:creator>c_dawg</dc:creator>
      <dc:date>2017-02-22T16:45:32Z</dc:date>
    </item>
    <item>
      <title>Re: What does production use to program boards?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-production-use-to-program-boards/m-p/661209#M13867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Colin,&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Please be sure the "Task Type" choose Kinetis :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14064i0CBCDE298748AC91/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. If still can not work , please tell me what version of your CW license , Professional ? Standard ? or Basic?&lt;/P&gt;&lt;P&gt;And also the code size .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 07:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-does-production-use-to-program-boards/m-p/661209#M13867</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-23T07:57:04Z</dc:date>
    </item>
  </channel>
</rss>