<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Help with the &amp;quot;Debug Database Initialization&amp;quot; message?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595042#M13351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I just installed CodeWarrior for MCU's in a laptop with Windows 10 (64 bit architecture) and at the moment I opened CodeWarrior I got the following message: "An internal error occurred during: Debug Database Initialization. java.lang.ExceptionInInitializerError". I tried removing the .metadata folder and also re-installing CodeWarrior but it didn't work. Any suggestions anybody? I would really appreciate it. I also attached the diagnostics file if it can be of any help.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338745"&gt;201609061259_DiagnosticInfo.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 07:36:06 GMT</pubDate>
    <dc:creator>javierhernandez</dc:creator>
    <dc:date>2016-09-06T07:36:06Z</dc:date>
    <item>
      <title>Help with the "Debug Database Initialization" message?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595042#M13351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I just installed CodeWarrior for MCU's in a laptop with Windows 10 (64 bit architecture) and at the moment I opened CodeWarrior I got the following message: "An internal error occurred during: Debug Database Initialization. java.lang.ExceptionInInitializerError". I tried removing the .metadata folder and also re-installing CodeWarrior but it didn't work. Any suggestions anybody? I would really appreciate it. I also attached the diagnostics file if it can be of any help.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338745"&gt;201609061259_DiagnosticInfo.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 07:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595042#M13351</guid>
      <dc:creator>javierhernandez</dc:creator>
      <dc:date>2016-09-06T07:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: Help with the "Debug Database Initialization" message?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595043#M13352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Javier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you logging on Windows with Administrator right? &amp;nbsp;Could you please install the CodeWarrior under the default path?&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.7&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Fiona Kuang&lt;BR /&gt;TIC - Technical Information Center&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 07:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595043#M13352</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2016-09-07T07:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: Help with the "Debug Database Initialization" message?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595044#M13353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In case it helps...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had a similar issue (same error) when I installed CodeWarrior 10.2 onto a Windows 7 x64 PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your workspace directory, under .metadata there is a log file with no name (just called ".log")&lt;/P&gt;&lt;P&gt;In that file I had the following error reported:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro" style="background: none #f6f6f6; border-left: 2px solid #cccccc; margin: 10px 0px; padding: 10px 20px;"&gt;&lt;P&gt;java.lang.UnsatisfiedLinkError: C:\Freescale\CW MCU v10.2\eclipse\plugins\com.freescale.core.debugger.ddd_7.18.0.FSL_b10910\DebugDatabase.dll: The application has failed to start because its side-by-side configuration is incorrect. Please see the application event log or use the command-line sxstrace.exe tool for more detail&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Side-by-side loading usually means that it expected something else to have been installed that is relied on.&lt;/P&gt;&lt;P&gt;I had to install the "Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)" - NOTE its the 32bit package, which can be downloaded from Microsoft here:&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://www.microsoft.com/en-us/download/details.aspx?id=5582" style="color: #2989c5;" title="https://www.microsoft.com/en-us/download/details.aspx?id=5582"&gt;Download Microsoft Visual C++ 2008 SP1 Redistributable Package (x86) from Official Microsoft Download Center&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once that was installed and I then restarted CodeWarrior the issue is no longer reported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Phil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 10:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595044#M13353</guid>
      <dc:creator>PhilV</dc:creator>
      <dc:date>2017-01-20T10:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: Help with the "Debug Database Initialization" message?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595045#M13354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you a lot Phil, I cannot tell you how happy I am now with your solution..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was getting the "cannot load debug database" error and also "Unknown Target Type" error and my "Target Types" list was empty.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This solved my error, I have un-installed all the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Microsoft Visual C++ Redistributable Package&lt;SPAN&gt;&amp;nbsp;versions and re-installed all the versions for both x86 and x64 and this worked!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Thank you again, thank you..&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Abdullah&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Dec 2018 07:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/595045#M13354</guid>
      <dc:creator>abdullahkahrama</dc:creator>
      <dc:date>2018-12-01T07:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: Help with the "Debug Database Initialization" message?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/1174667#M15490</link>
      <description>&lt;P&gt;Hello Phil,&lt;/P&gt;&lt;P&gt;many thanks. I had the same problem&amp;nbsp; after installing CW 11V1. After downloading the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;"Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)" from microsoft and repairing the package that was installed with CW, everything worked fine.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks again.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;John&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 17:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Help-with-the-quot-Debug-Database-Initialization-quot-message/m-p/1174667#M15490</guid>
      <dc:creator>jgerhardy</dc:creator>
      <dc:date>2020-10-28T17:20:04Z</dc:date>
    </item>
  </channel>
</rss>