<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックHow to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571907#M13209</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an MPC8280-based system with a convoluted build process I haven't figures out yet.&amp;nbsp; I'd like to use my CodeWarrior TAP, driven by CodeWarrior for PowerQUICC 8.8, first to just read the contents of RAM and flash, and I don't see how to do that.&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2016 14:25:08 GMT</pubDate>
    <dc:creator>gschmick</dc:creator>
    <dc:date>2016-06-24T14:25:08Z</dc:date>
    <item>
      <title>How to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571907#M13209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an MPC8280-based system with a convoluted build process I haven't figures out yet.&amp;nbsp; I'd like to use my CodeWarrior TAP, driven by CodeWarrior for PowerQUICC 8.8, first to just read the contents of RAM and flash, and I don't see how to do that.&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 14:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571907#M13209</guid>
      <dc:creator>gschmick</dc:creator>
      <dc:date>2016-06-24T14:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571908#M13210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Grant Schmick,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Please follow new project wizards to create a bare board project for MPC8280 platform, then modify the initiation file in C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Support\Initialization_Files\PQ2 according to your target board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Connect CodeWarrior to the target board from Debug-&amp;gt;Connect, then read RAM memory from Debug-&amp;gt;EPPC-&amp;gt;Load/Save Memory.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 08:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571908#M13210</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-06-28T08:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571909#M13211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yiping,&lt;/P&gt;&lt;P&gt;Thanks for the advice.&amp;nbsp; I tried this, got thru the wizard but there was no mention of the initialization file, so I'm not sure how it's specified.&amp;nbsp; Do I have to create one with the name of my project?&amp;nbsp; Also, looking at the examples, it's not clear what may be needed in my init file.&amp;nbsp; Any advice or reference I can read?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, I tried the Load/Save Memory dialog, but the "OK" button stayed grayed out, though I think I used a valid address (flash).&amp;nbsp; any thoughts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Grant&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 20:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571909#M13211</guid>
      <dc:creator>gschmick</dc:creator>
      <dc:date>2016-06-29T20:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571910#M13212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Grant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could specify the initialization file from Edit-&amp;gt;Debug Version Setting-&amp;gt;Debugger-&amp;gt;EPPC Debugger Setting-&amp;gt;Use Target Initialization. CodeWarrior initialization files for MPC8280 are located in C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Support\Initialization_Files\PQ2, you could choose one porting for your board, please check the section "Setup the chip selects".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After CodeWarrior connects to the target board from Debug-&amp;gt;Connect, "Load/Save Memory" would be available in CodeWarrior IDE.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 09:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/571910#M13212</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-06-30T09:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to read memory using CodeWarrior TAP/CW for PowerQUICC w/o source/executable.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/2087821#M16091</link>
      <description>&lt;P&gt;Hi. how to read Nand-flash dump? and how to write it to another board with the same processor and memory chip?&lt;/P&gt;</description>
      <pubDate>Sun, 27 Apr 2025 22:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-read-memory-using-CodeWarrior-TAP-CW-for-PowerQUICC-w-o/m-p/2087821#M16091</guid>
      <dc:creator>Zavr</dc:creator>
      <dc:date>2025-04-27T22:09:42Z</dc:date>
    </item>
  </channel>
</rss>