<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Duplicated target tasks</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541210#M13041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I do that then the .ttf file is no longer under version control, so moving the file is not an option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The file is in this location: {workspace}\app_NGUC_SingleBoard_52258\Project_Settings\Debugger\NGUC_mcf52258.ttf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please explain why CW copies the file? I want to stop this behavior, not work around it. There's no reason for this to happen. Is there some setting which prevents this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I am not repeatedly closing then opening the project. Even if I were, why would this cause the task to be copied?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jun 2016 14:09:45 GMT</pubDate>
    <dc:creator>frankbaird</dc:creator>
    <dc:date>2016-06-17T14:09:45Z</dc:date>
    <item>
      <title>Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541207#M13038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior 10.6.4. After a while of performing several debugging runs, I find that my target task has become duplicated many times. In the attached image, only the top task "NGUC_mcf52258" is actually needed. All the rest are duplicates which are somehow being created. Why is the task being duplicated, and how do I stop it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="153778_153778.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121817i48699FFD6D0DD4B4/image-size/large?v=v2&amp;amp;px=999" role="button" title="153778_153778.png" alt="153778_153778.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59750i6AD2386EDF80E1BB/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 22:08:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541207#M13038</guid>
      <dc:creator>frankbaird</dc:creator>
      <dc:date>2016-06-16T22:08:08Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541208#M13039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frank,&lt;/P&gt;&lt;P&gt;Please click once the task , then click the "x" to delete :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59841i8EBD1DD7DAB6F679/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 01:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541208#M13039</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-17T01:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541209#M13040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason which show so many is you repeat close your project, the re-open it .&lt;/P&gt;&lt;P&gt;The workaround is transfer the *.ttf files to other place not under the project .&lt;/P&gt;&lt;P&gt;For example , under your project folder ,you can find "GUNC_mcf52258.ttf" file,&lt;/P&gt;&lt;P&gt;cut and past it to the desktop , then no matter how many time you repeat open the project ,&lt;/P&gt;&lt;P&gt;it won't add so many Tasks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 05:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541209#M13040</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-17T05:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541210#M13041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I do that then the .ttf file is no longer under version control, so moving the file is not an option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The file is in this location: {workspace}\app_NGUC_SingleBoard_52258\Project_Settings\Debugger\NGUC_mcf52258.ttf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please explain why CW copies the file? I want to stop this behavior, not work around it. There's no reason for this to happen. Is there some setting which prevents this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I am not repeatedly closing then opening the project. Even if I were, why would this cause the task to be copied?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 14:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541210#M13041</guid>
      <dc:creator>frankbaird</dc:creator>
      <dc:date>2016-06-17T14:09:45Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541211#M13042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know how this question was marked as Assumed Answered. I don't remember marking it in any way. If a forum mod did this, please remove it. This question is not answered.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 19:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541211#M13042</guid>
      <dc:creator>frankbaird</dc:creator>
      <dc:date>2016-06-17T19:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: Duplicated target tasks</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541212#M13043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frank,&lt;/P&gt;&lt;P&gt;I have checked again , under the “AutoFlsh”, when reopen the project or CW,&lt;/P&gt;&lt;P&gt;it will not add too much tasks .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60250i4E813345D8392537/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please delete all of your tasks , then have a try , check whether it will add other tasks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And under Root, when open the CW again, it will add one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 10:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Duplicated-target-tasks/m-p/541212#M13043</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-20T10:41:02Z</dc:date>
    </item>
  </channel>
</rss>