<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Compiler Errors in HCS08 Configuration</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538684#M13033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The chip used is MC9S08GT60 . The configuration for HCS08 is selected from the drop down men which also has FLASH Configuration. I got to know the overlap definition at the same address and when i fixed those erros, it shows a error regardinng allocation of ROM going out of space,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The definition overlap was due to the errors since some variables was defined explicitly defined with address in .c files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my question is whether the same PRM File cannot be used for both FLASH and HCSO8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know the difference between HCS08 configuration and FLASH configuration.Whether the HCS08 configuration is used for debugging ?Whether FLASH configuration can be used for debugging.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jul 2016 15:35:38 GMT</pubDate>
    <dc:creator>preetuabraham</dc:creator>
    <dc:date>2016-07-26T15:35:38Z</dc:date>
    <item>
      <title>Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538682#M13031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt; I would like to know the difference between HCS08 configuration and FLASH configuration.Whether the HCS08 configuration is used for debugging ?Whether FLASH configuration can be used for debugging.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For my project,when I tried to build and compiler ,it gives erros for HCS08 configuration for overlapping of segments.Please find the attachment ,but when I compile with FLASH Configuration for the same .prm file ,it does not give erros and produces a .sx file.Whether there any specific settings apart of changing the configuration&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 18:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538682#M13031</guid>
      <dc:creator>preetuabraham</dc:creator>
      <dc:date>2016-07-25T18:10:29Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538683#M13032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Preetu,&lt;/P&gt;&lt;P&gt;From the error , in generally there maybe some definition overlap at the same address ,&lt;/P&gt;&lt;P&gt;please check these address &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38017i0233044088703678/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you have not checked it out, you can also send your project to me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 07:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538683#M13032</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-07-26T07:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538684#M13033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The chip used is MC9S08GT60 . The configuration for HCS08 is selected from the drop down men which also has FLASH Configuration. I got to know the overlap definition at the same address and when i fixed those erros, it shows a error regardinng allocation of ROM going out of space,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The definition overlap was due to the errors since some variables was defined explicitly defined with address in .c files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my question is whether the same PRM File cannot be used for both FLASH and HCSO8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know the difference between HCS08 configuration and FLASH configuration.Whether the HCS08 configuration is used for debugging ?Whether FLASH configuration can be used for debugging.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 15:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538684#M13033</guid>
      <dc:creator>preetuabraham</dc:creator>
      <dc:date>2016-07-26T15:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538685#M13034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Preetu,&lt;/P&gt;&lt;P&gt;From your screenshot i think maybe you use the CW 10.6 , right ?&lt;/P&gt;&lt;P&gt;If yes , when we create one HCS08 project ,the default configuration is Flash configuration,&lt;/P&gt;&lt;P&gt;there is no HSC08 configuration&amp;nbsp; :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37607i089996C88F5317CE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So the HCS08 configuration is configured by customer ,&amp;nbsp; from check the contents&amp;nbsp; between the two&lt;/P&gt;&lt;P&gt;configuration to the difference :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37640iDC186014584A863A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 06:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538685#M13034</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-07-27T06:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538686#M13035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;Yes I am using 10.6.4 and the starting configuration is Flash&lt;/P&gt;&lt;P&gt;We can set the HCS08 configuration under the option Manage configuration&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 15:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538686#M13035</guid>
      <dc:creator>preetuabraham</dc:creator>
      <dc:date>2016-07-27T15:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538687#M13036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40296i0A2EB03BB64B2379/image-size/large?v=v2&amp;amp;px=999" title="HCS08_2.jpg" alt="HCS08_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 15:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538687#M13036</guid>
      <dc:creator>preetuabraham</dc:creator>
      <dc:date>2016-07-27T15:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler Errors in HCS08 Configuration</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538688#M13037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Preetu,&lt;/P&gt;&lt;P&gt;This HCS08 configuration is just a basic configuration ,&lt;/P&gt;&lt;P&gt;it need configured by customer refer to customers' demand .&lt;/P&gt;&lt;P&gt;If only select it ,&amp;nbsp; then configure nothing,&amp;nbsp; when build , it will show error .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example , you can create one simple&amp;nbsp; project to have a try ,&lt;/P&gt;&lt;P&gt;in the "HCS08 compiler" selection , the HCS08 configuration have not include all the&lt;/P&gt;&lt;P&gt;header files :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42089i8A5B568EE6FB1CF7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42148i6379EC59A3B8931F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I recommend you use the FLASH configuration .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 03:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Compiler-Errors-in-HCS08-Configuration/m-p/538688#M13037</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-07-28T03:50:59Z</dc:date>
    </item>
  </channel>
</rss>