<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132590#M1285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Are&amp;nbsp; you using an LPT interface interface module?&amp;nbsp; Like the BDM-Multilink?&amp;nbsp; There's a patch that needs to be done so that XP won't poll the LPT port.&amp;nbsp; (I got a program from Metroworks to create a registry entry to fix the issue)&lt;/P&gt;&lt;P&gt;But I've not heard of that locking up a machine.&amp;nbsp; Just causing BDM communication errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Apr 2006 19:47:34 GMT</pubDate>
    <dc:creator>mke_et</dc:creator>
    <dc:date>2006-04-18T19:47:34Z</dc:date>
    <item>
      <title>Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132587#M1282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have CodeWarrior V3.1 and V5.0 installed at my home computer which has Windows XP home edition.&amp;nbsp; The IDE and simulation work fine, but the ICD/Multlinke lock up when started.&amp;nbsp; The ICD assistant windows never&amp;nbsp;displays.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please tell me if you are not having problems with the XP Home Edition.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Again, please reply because I haven't used the DEMO9S08QG8 board yet.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2006 00:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132587#M1282</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2006-04-17T00:09:49Z</dc:date>
    </item>
    <item>
      <title>Re: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132588#M1283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi FC,&lt;/P&gt;&lt;P&gt;I have CW3.1 and 5 both loaded on to a XP Pro machine and a XP home machine and I don't have any problems or notice any difference.&lt;/P&gt;&lt;P&gt;BR Peg&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2006 06:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132588#M1283</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-04-17T06:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132589#M1284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Thank you for verifying this.&amp;nbsp; This means I have some corrupt system files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2006 09:09:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132589#M1284</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2006-04-17T09:09:51Z</dc:date>
    </item>
    <item>
      <title>Re: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132590#M1285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Are&amp;nbsp; you using an LPT interface interface module?&amp;nbsp; Like the BDM-Multilink?&amp;nbsp; There's a patch that needs to be done so that XP won't poll the LPT port.&amp;nbsp; (I got a program from Metroworks to create a registry entry to fix the issue)&lt;/P&gt;&lt;P&gt;But I've not heard of that locking up a machine.&amp;nbsp; Just causing BDM communication errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2006 19:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132590#M1285</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2006-04-18T19:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132591#M1286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The target is the DEMO9S08QG8 demo board using the USB Multilink.&amp;nbsp; The debugger locks up when in circuit debug mode.&amp;nbsp; The ICD assistant window never shows up.&amp;nbsp; It seems like hiwave.exe cannot find a file.&amp;nbsp;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2006 11:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132591#M1286</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2006-04-20T11:35:10Z</dc:date>
    </item>
    <item>
      <title>Re: Is Windows XP Home Edition not compatible with CodeWarrior V3.1 and V5.0 ?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132592#M1287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi FC,&lt;/P&gt;&lt;P&gt;Just for you, I just flashed and ran a project into my recently built "home made" DEMO9S08QG8 board using my XP home laptop and&amp;nbsp;CW5 through a P&amp;amp;E USB Multilink all with no dramas.&lt;/P&gt;&lt;P&gt;BR Peg&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2006 19:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Is-Windows-XP-Home-Edition-not-compatible-with-CodeWarrior-V3-1/m-p/132592#M1287</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-04-20T19:29:40Z</dc:date>
    </item>
  </channel>
</rss>